ubuntu rootfs with frame buffer support for imx6 devices

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

ubuntu rootfs with frame buffer support for imx6 devices

1,742件の閲覧回数
srinivasaporam
Contributor II

Hi,

We have got imx6 Q, DL reference boards with us. When we are trying to port ubuntu, then xorg is failing. When we are giving 'startx' command then we are getting following error:

segmentation fault at 0x0

connection refused

Where as when we are trying with Debian rootfs, it is working fine.

is there any issue with ubuntu rootfs. can anybody post the  working ubuntu rootfs to work with 3.14 kernel.

ラベル(4)
タグ(1)
0 件の賞賛
返信
1 返信

1,502件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi srinivasa

nxp does not provide ubuntu, one can look at efforts on

i.MX6 SABRE Lite - Linux on ARM - eewiki

http://boundarydevices.com/trusty-ubuntu-mx6/

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信