ubuntu on IMX8M

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ubuntu on IMX8M

7,398 Views
conradcoetzee
Contributor I

HI,

Would it possible to have Ubuntu Linux on the new IMX8M, It seems to be a more supported linux distri with the likes of beagle bone and rasberri PI.

Regards

Conrad

0 Kudos
Reply
4 Replies

5,422 Views
gary_bisson
Senior Contributor III

Hi Conrad,

Boundary Devices provides Ubuntu & Debian images for all i.MX processors:

Ubuntu Bionic 18.04 LTS for Nitrogen8M board – September 2018 (kernel 4.9.x) - Boundary Devices 

Hope you'll find a platform that fits your need here:

https://boundarydevices.com/product-category/popular-sbc-and-som-modules/ 

Regards,

Gary

0 Kudos
Reply

5,422 Views
conradcoetzee
Contributor I

Hi Gary,

Thanks for the feedback, I will investigate the links

Kind Regards

Conrad Coetzee (B-Tech Eng.)

Engineer: Field Application & PLM

Altron Arrow

+27 (0) 11 923 9720

+27 (0) 83 746 2616

0 Kudos
Reply

5,422 Views
diegoadrian
NXP Employee
NXP Employee

Hello,

Unfortunately, we do not have support for Ubuntu in all of our i.MX devices. I apologize for the inconveniences this could give you.

Best Regards,

Diego.

0 Kudos
Reply

5,422 Views
conradcoetzee
Contributor I

Hi Diego,

Thanks for the response,

What I was actually looking at was the support for a Debian style Linux. I only used ubuntu as a example as it is based on Debian.

Would there be a chance of future plans for the Debian style linux ?

Kind Regards

Conrad Coetzee (B-Tech Eng.)

Engineer: Field Application & PLM

Altron Arrow

+27 (0) 11 923 9720

+27 (0) 83 746 2616

0 Kudos
Reply