uboot-imx atheros PHY driver config question?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

uboot-imx atheros PHY driver config question?

2,405 Views
kenlin
Contributor II

Hi,

 

 

We encountered the voltage peak issue while doing the IEEE PHY conformance test, which has to do with the AR8033 register (SetDes Test and System Mode Control) setting in u-boot. After looking into the commit info (from git://git.freescale.com/imx/uboot-imx.git, branch l5.1.1_2.1.0-ga ), we found the PHY configuration has to do with the following commits, which are from NXP developers.

 

Is there's anyone from NXP who can help explain why the register SerDES test and System Mode control is set to 0x3D47 learned from Andy Fleming commit info? When we checked the AR8033 spec (see the attachment), it is said the reserved bits would be set to 0 after a HW or SW reset.

 

Thank you

 

 

commit 9082eeac5de1335d663016668c9b89c290f5c79b
Author: Andy Fleming <afleming@freescale.com>
Date: Thu Apr 7 21:56:05 2011 -0500

phylib: Add a bunch of PHY drivers from tsec

The tsec driver had a bunch of PHY drivers already written. This
converts them all into PHY Lib drivers, and serves as the first
set of PHY drivers for PHY Lib.

While doing that, cleaned up a number of magic numbers (though
not all of them, as PHY vendors like to keep their numbers as
magical as possible). Also, noticed that almost all of the
vitesse/cicada PHYs had the same config/parse/startup functions,
so those have been collapsed into one.

Signed-off-by: Andy Fleming <afleming@freescale.com>
Signed-off-by: Kumar Gala <galak@kernel.crashing.org>
Acked-by: Detlev Zundel <dzu@denx.de>

 

+/*
+ * Atheros PHY drivers
+ *
+ * This program is free software; you can redistribute it and/or
+ * modify it under the terms of the GNU General Public License as
+ * published by the Free Software Foundation; either version 2 of
+ * the License, or (at your option) any later version.
+ *
+ * This program is distributed in the hope that it will be useful,
+ * but WITHOUT ANY WARRANTY; without even the implied warranty of
+ * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the
+ * GNU General Public License for more details.
+ *
+ * You should have received a copy of the GNU General Public License
+ * along with this program; if not, write to the Free Software
+ * Foundation, Inc., 59 Temple Place, Suite 330, Boston,
+ * MA 02111-1307 USA
+ *
+ * Copyright 2011 Freescale Semiconductor, Inc.
+ * author Andy Fleming
+ *
+ */
+#include <phy.h>
+
+static int ar8021_config(struct phy_device *phydev)
+{
+ phy_write(phydev, MDIO_DEVAD_NONE, 0x1d, 0x05);
+ phy_write(phydev, MDIO_DEVAD_NONE, 0x1e, 0x3D47);
+
+ return 0;
+}
+
+struct phy_driver AR8021_driver = {
+ .name = "AR8021",
+ .uid = 0x4dd040,
+ .mask = 0xfffff0,
+ .features = PHY_GBIT_FEATURES,
+ .config = ar8021_config,
+ .startup = genphy_startup,
+ .shutdown = genphy_shutdown,
+};
+
+int phy_atheros_init(void)
+{
+ phy_register(&AR8021_driver);
+
+ return 0;
+}

 

 

commit 626ee1e32eeb4fc89e0f406d6067ed6e71d8302f
Author: Shengzhou Liu <Shengzhou.Liu@freescale.com>
Date: Thu Aug 8 16:33:35 2013 +0800

phylib: update atheros ar803x phy

As AR8031 and AR8033 have same PHY ID 0x4dd074, they use the
common driver. Currently AR8031_driver didn't work for AR8033,
hence updated it to have it work on AR8031/AR8033.

Signed-off-by: Shengzhou Liu <Shengzhou.Liu@freescale.com>

diff --git a/drivers/net/phy/atheros.c b/drivers/net/phy/atheros.c
index 0f2dfd6..7a1453f 100644
--- a/drivers/net/phy/atheros.c
+++ b/drivers/net/phy/atheros.c
@@ -48,11 +48,11 @@ static struct phy_driver AR8021_driver = {
};

static struct phy_driver AR8031_driver = {
- .name = "AR8031",
+ .name = "AR8031/AR8033",
.uid = 0x4dd074,
.mask = 0xfffff0,
.features = PHY_GBIT_FEATURES,
- .config = genphy_config,
+ .config = ar8021_config,
.startup = genphy_startup,
.shutdown = genphy_shutdown,
};

Labels (5)
Tags (1)
0 Kudos
Reply
0 Replies