uboot->fastboot command error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

uboot->fastboot command error

1,543 Views
sunyd
Contributor I
hi,buddy
clipboardwps图片.png
when i input command "fastboot"  ,but error that  info of  above image
 i check the code,and like that
pastedImage_2.png

pastedImage_1.png

but ,and i don't know how to reslove it, please help me

thank you !!!

Labels (1)
0 Kudos
Reply
1 Reply

1,272 Views
igorpadykov
NXP Employee
NXP Employee

Hi sunyd

one can look at description on

Factory flashing with U-Boot and fastboot on Freescale i.MX6 

Use nxp uboot from source.codeaurora.org/external/imx repository and

verify that there is "#define CONFIG_FASTBOOT" in

uboot/include/configs/mx6sabre_common.h

mx6sabre_common.h\configs\include - uboot-imx - i.MX U-Boot 

uboot-imx - i.MX U-Boot 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply