uboot for NAND flash

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,212件の閲覧回数
jimmychiang
Contributor III

Dear Sir!

I have a MCIMX7SABRE EVB.

I tried build U-Boot and Kernel in standalone environment.

And I refer to the imx-yocto-L5.4.70_2.3.0 doc, and the compilation environment has been established.

However, because I need to boot from NAND flash. So I tried to compile with the following instructions.

=============================================================

Download source by cloning with git clone https://source.codeaurora.org/external/imx/linux-imx -b
imx_5.4.70_2.3.0
cd linux-imx
make imx_v7_defconfig
make

=============================================================

But the "imx_v7_defconfig" file has no NAND Flash configuration. 

In fact, I have used "mfgtools\Profiles\Linux\OS Firmware\firmware\u-boot-imx7dsabresd_nand.imx" and program to NAND flash, it is working on MCIMX7SABRE-EVB.

So I think there should be a configuration file for "u-boot-imx7dsabresd_nand.imx".

However, there are many configuration files in uboot source code. (in "uboot-imx\configs" path)

Could you help me and let me know which configuration can be used for NAND boot on MCIMX7SABRE-EVB?

 

Thanks!

ラベル(1)
0 件の賞賛
返信
1 解決策
2,203件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi

 

for uboot configuration one can look at sect.5.5 U-Boot configuration i.MX Yocto Project User’s Guide​

 

Best regards
igor

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,204件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi

 

for uboot configuration one can look at sect.5.5 U-Boot configuration i.MX Yocto Project User’s Guide​

 

Best regards
igor

0 件の賞賛
返信