uart sharing

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

uart sharing

1,743 Views
o_scherbinin
Contributor III

Hello everybody.
There is the need to share one uart for A9(linux) & M4(FreeRTOS) cores (imx6sx).
Could you give me right direction to solve the porblem.
Regards.

0 Kudos
Reply
1 Reply

1,608 Views
igorpadykov
NXP Employee
NXP Employee

Hi Oleg

one can try to set permissions with RDC described in

Chapter 52 Resource Domain Controller (RDC)  i.MX6SX Reference Manual
http://www.nxp.com/docs/en/reference-manual/IMX6SXRM.pdf

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------