uart sharing

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

uart sharing

1,744件の閲覧回数
o_scherbinin
Contributor III

Hello everybody.
There is the need to share one uart for A9(linux) & M4(FreeRTOS) cores (imx6sx).
Could you give me right direction to solve the porblem.
Regards.

0 件の賞賛
返信
1 返信

1,609件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Oleg

one can try to set permissions with RDC described in

Chapter 52 Resource Domain Controller (RDC)  i.MX6SX Reference Manual
http://www.nxp.com/docs/en/reference-manual/IMX6SXRM.pdf

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------