uSDHC3 Booting

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

uSDHC3 Booting

2,767件の閲覧回数
niteshsahay
Contributor III

Hi 

I am using iMX6DL for my application.

For booting from SD card i have considered as uSDHC3 interface but my board is not getting booted

In one of the evaluation board, which is connected to uSDHC1 is getting booted .

I have done the configuration for my board as below :

BOOT_CFG2[4:3] ---  10.

Can anyone let me know the possible reason for such occurrence.

Regards

Nitesh

ラベル(1)
0 件の賞賛
返信
1 返信

2,647件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Nitesh

please check with oscilloscope if signals are present on SD and

try to prolong POR up to 0.8-1 sec. Also recommended to attach jtag

debugger and check boot settings in SRC_SBMR1,2 register, they are

decribed in Chapter 60 System Reset Controller (SRC).

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信