uImage booting problem.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

uImage booting problem.

3,301件の閲覧回数
shreenidhiachar
Contributor I

Hi,

     I have been working in  custom board of imx6sl . My boot loader is loading fine but when it tries to boot uImage , the booting stops after "DVFS driver module loaded" print. It is also my first experience in BSP work. So please anybody know the solution for this, answer me . I also added the my boot print here..

U-Boot 2009.08-00693-g4a6b27b-dirty (Mar 03 2014 - 17:12:28)                

                                                                            

CPU: Freescale i.MX6 family TO1.2 at 792 MHz                                

Thermal sensor with ratio = 178        

Temperature:   31 C, calibration data 0x5674db69

mx6q pll1: 792MHz                      

mx6q pll2: 528MHz                      

mx6q pll3: 480MHz                      

mx6q pll8: 50MHz                       

ipg clock     : 66000000Hz

ipg per clock : 66000000Hz

uart clock    : 80000000Hz

cspi clock    : 60000000Hz

ahb clock     : 132000000Hz

axi clock   : 198000000Hz

emi_slow clock: 99000000Hz

ddr clock     : 396000000Hz

usdhc1 clock  : 198000000Hz

usdhc2 clock  : 198000000Hz

usdhc3 clock  : 198000000Hz

usdhc4 clock  : 198000000Hz

Board: MX6SoloLite-EVK (0x60312): [ POR ]

Boot Device: SD

I2C:   ready

DRAM:   1 GB

MMC:   FSL_USDHC: 0,FSL_USDHC: 1,FSL_USDHC: 2

*** Warning - bad CRC or MMC, using default environment

In:    serial

Out:   serial

Err:   serial

Found PFUZE100! deviceid=10,revid=21

Net:   got MAC address from IIM: 00:00:00:00:00:00

FEC0 [PRIME]

Hit any key to stop autoboot:  0

mmc2 is current device

MMC read: dev # 2, block # 2048, count 8192 ... 8192 blocks read: OK

## Booting kernel from Legacy Image at 80800000 ...

   Image Name:   Linux-3.0.35-2666-gbdde708

   Image Type:   ARM Linux Kernel Image (uncompressed)

   Data Size:    3585076 Bytes =  3.4 MB

   Load Address: 80008000

   Entry Point:  80008000

   Verifying Checksum ... OK

   Loading Kernel Image ... OK

OK

Starting kernel ...

Linux version 3.0.35-2666-gbdde708 (shreenidhi@PC57) (gcc version 4.6.2 20110630 (prerelease) (Freescale MAD -- Linaro 2011.07 -4

CPU: ARMv7 Processor [412fc09a] revision 10 (ARMv7), cr=10c53c7d

CPU: VIPT nonaliasing data cache, VIPT aliasing instruction cache

Machine: Freescale i.MX 6SoloLite EVK Board

Memory policy: ECC disabled, Data cache writeback

CPU identified as i.MX6SoloLite, silicon rev 1.2

Built 1 zonelists in Zone order, mobility grouping on.  Total pages: 251904

Kernel command line: console=ttymxc0,115200 root=/dev/mmcblk0p1 rootwait

PID hash table entries: 4096 (order: 2, 16384 bytes)

Dentry cache hash table entries: 131072 (order: 7, 524288 bytes)

Inode-cache hash table entries: 65536 (order: 6, 262144 bytes)

Memory: 992MB = 992MB total

Memory: 995848k/995848k available, 52728k reserved, 0K highmem

Virtual kernel memory layout:

    vector  : 0xffff0000 - 0xffff1000   (   4 kB)

    fixmap  : 0xfff00000 - 0xfffe0000   ( 896 kB)

    DMA     : 0xf4600000 - 0xffe00000   ( 184 MB)

    vmalloc : 0xc0800000 - 0xf2000000   ( 792 MB)

    lowmem  : 0x80000000 - 0xc0000000   (1024 MB)

    pkmap   : 0x7fe00000 - 0x80000000   (   2 MB)

    modules : 0x7f000000 - 0x7fe00000   (  14 MB)

      .init : 0x80008000 - 0x80035000   ( 180 kB)

      .text : 0x80035000 - 0x80a30c1c   (10224 kB)

      .data : 0x80a32000 - 0x80a86740   ( 338 kB)

       .bss : 0x80a86764 - 0x80aab6f8   ( 148 kB)

SLUB: Genslabs=13, HWalign=32, Order=0-3, MinObjects=0, CPUs=1, Nodes=1

Preemptible hierarchical RCU implementation.

NR_IRQS:624

MXC GPIO hardware

sched_clock: 32 bits at 24MHz, resolution 41ns, wraps every 178956ms

arm_max_freq=1GHz

MXC_Early serial console at MMIO 0x2020000 (options '115200')

bootconsole [ttymxc0] enabled

Console: colour dummy device 80x30

Calibrating delay loop... 1581.05 BogoMIPS (lpj=7905280)

pid_max: default: 32768 minimum: 301

Mount-cache hash table entries: 512

CPU: Testing write buffer coherency: ok

hw perfevents: enabled with ARMv7 Cortex-A9 PMU driver, 7 counters available

print_constraints: dummy:

NET: Registered protocol family 16

print_constraints: vddpu: 725 <--> 1300 mV at 700 mV fast normal

print_constraints: vddcore: 725 <--> 1300 mV at 1100 mV fast normal

print_constraints: vddsoc: 725 <--> 1300 mV at 1200 mV fast normal

print_constraints: vdd2p5: 2000 <--> 2775 mV at 2400 mV fast normal

print_constraints: vdd1p1: 800 <--> 1400 mV at 1100 mV fast normal

print_constraints: vdd3p0: 2625 <--> 3400 mV at 3000 mV fast normal

hw-breakpoint: found 6 breakpoint and 1 watchpoint registers.

hw-breakpoint: 1 breakpoint(s) reserved for watchpoint single-step.

hw-breakpoint: maximum watchpoint size is 4 bytes.

L310 cache controller enabled

l2x0: 16 ways, CACHE_ID 0x410000c8, AUX_CTRL 0x02030000, Cache size: 262144 B

bio: create slab <bio-0> at 0

print_constraints: vmmc: 3300 mV

print_constraints: SPKVDD: 4325 mV

SCSI subsystem initialized

spi_imx imx6q-ecspi.0: probed

usbcore: registered new interface driver usbfs

usbcore: registered new interface driver hub

usbcore: registered new device driver usb

Freescale USB OTG Driver loaded, $Revision: 1.55 $

mc_pfuze 0-0008: ID: 0,Full lay: 2 ,Metal lay: 1

mc_pfuze 0-0008: FAB: 0 ,FIN: 0

print_constraints: PFUZE100_SW1A: 300 <--> 1875 mV at 1300 mV

print_constraints: PFUZE100_SW1B: 300 <--> 1875 mV at 300 mV

print_constraints: PFUZE100_SW1C: 300 <--> 1875 mV at 1300 mV

print_constraints: PFUZE100_SW2: 800 <--> 3950 mV at 3150 mV

print_constraints: PFUZE100_SW3A: 400 <--> 1975 mV at 1500 mV

print_constraints: PFUZE100_SW3B: 400 <--> 1975 mV at 1500 mV

print_constraints: PFUZE100_SW4: 800 <--> 3950 mV at 3300 mV

print_constraints: PFUZE100_SWBST: 5000 <--> 5150 mV at 5000 mV

print_constraints: PFUZE100_VSNVS: 1200 <--> 3000 mV at 1800 mV

print_constraints: PFUZE100_VREFDDR: at 750 mV

print_constraints: PFUZE100_VGEN1: 800 <--> 1550 mV at 1200 mV

print_constraints: PFUZE100_VGEN2: 800 <--> 1550 mV at 1500 mV

print_constraints: PFUZE100_VGEN3: 1800 <--> 3300 mV at 1800 mV

print_constraints: PFUZE100_VGEN4: 1800 <--> 3300 mV at 1800 mV

print_constraints: PFUZE100_VGEN5: 1800 <--> 3300 mV at 2500 mV

print_constraints: PFUZE100_VGEN6: 1800 <--> 3300 mV at 2800 mV

i2c i2c-1: Invalid 7-bit I2C address 0x00

i2c i2c-1: Can't create device at 0x00

MIPI CSI2 driver module loaded

Advanced Linux Sound Architecture Driver Version 1.0.24.

Bluetooth: Core ver 2.16

NET: Registered protocol family 31

Bluetooth: HCI device and connection manager initialized

Bluetooth: HCI socket layer initialized

Bluetooth: L2CAP socket layer initialized

Bluetooth: SCO socket layer initialized

cfg80211: Calling CRDA to update world regulatory domain

max17135 0-0048: Max17135 PMIC not found!

max17135 regulator init failed: -6

i2c-core: driver [max17135] using legacy suspend method

i2c-core: driver [max17135] using legacy resume method

Switching to clocksource mxc_timer1

NET: Registered protocol family 2

IP route cache hash table entries: 32768 (order: 5, 131072 bytes)

TCP established hash table entries: 131072 (order: 8, 1048576 bytes)

TCP bind hash table entries: 65536 (order: 6, 262144 bytes)

TCP: Hash tables configured (established 131072 bind 65536)

TCP reno registered

UDP hash table entries: 512 (order: 1, 8192 bytes)

UDP-Lite hash table entries: 512 (order: 1, 8192 bytes)

NET: Registered protocol family 1

RPC: Registered named UNIX socket transport module.

RPC: Registered udp transport module.

RPC: Registered tcp transport module.

RPC: Registered tcp NFSv4.1 backchannel transport module.

etb: probe of etb failed with error -2

etm: probe of etm.0 failed with error -2

Static Power Management for Freescale i.MX6

wait mode is enabled for i.MX6

cpaddr = c0820000 suspend_iram_base=c0840000

PM driver module loaded

IMX usb wakeup probe

add wake up source irq 75

IMX usb wakeup probe

mxc_bt_rfkill driver success loaded

rfkill: BT RF going to : on

cpu regulator mode:ldo_bypass

_regulator_get: get() with no identifier

mx6_cpu_regulator_init: failed to get pu regulator

i.MXC CPU frequency driver

JFFS2 version 2.2. (NAND) �© 2001-2006 Red Hat, Inc.

msgmni has been set to 1945

io scheduler noop registered

io scheduler deadline registered

io scheduler cfq registered (default)

Console: switching to colour frame buffer device 100x30

imx-sdma imx-sdma: loaded firmware 1.1

imx-sdma imx-sdma: initialized

Serial: IMX driver

imx-uart.0: ttymxc0 at MMIO 0x2020000 (irq = 58) is a IMX

console [ttymxc0] enabled, bootconsole disabled

console [ttymxc0] enabled, bootconsole disabled

fsl_rngc fsl_rngc.0: FSL RNGC Registered.

loop: module loaded

m25p80 spi0.0: found m25p05-nonjedec, expected m25p32

m25p80 spi0.0: m25p05-nonjedec (64 Kbytes)

Creating 2 MTD partitions on "m25p32":

0x000000000000-0x000000100000 : "bootloader"

mtd: partition "bootloader" extends beyond the end of device "m25p32" -- size truncated to 0x10000

0x000000010000-0x000000010000 : "kernel"

mtd: partition "kernel" is out of reach -- disabled

vcan: Virtual CAN interface driver

CAN device driver interface

flexcan netdevice driver

FEC Ethernet Driver

fec_enet_mii_bus: probed

ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver

fsl-ehci fsl-ehci.0: Freescale On-Chip EHCI Host Controller

fsl-ehci fsl-ehci.0: new USB bus registered, assigned bus number 1

fsl-ehci fsl-ehci.0: irq 75, io base 0x02184000

fsl-ehci fsl-ehci.0: USB 2.0 started, EHCI 1.00

hub 1-0:1.0: USB hub found

hub 1-0:1.0: 1 port detected

add wake up source irq 74

fsl-ehci fsl-ehci.1: Freescale On-Chip EHCI Host Controller

fsl-ehci fsl-ehci.1: new USB bus registered, assigned bus number 2

fsl-ehci fsl-ehci.1: irq 74, io base 0x02184200

fsl-ehci fsl-ehci.1: USB 2.0 started, EHCI 1.00

hub 2-0:1.0: USB hub found

hub 2-0:1.0: 1 port detected

Initializing USB Mass Storage driver...

usbcore: registered new interface driver usb-storage

USB Mass Storage support registered.

ARC USBOTG Device Controller driver (1 August 2005)

mousedev: PS/2 mouse device common for all mice

input: imx-keypad as /devices/platform/imx-keypad/input/input0

elan - Read Hello Packet Failed

elan-touch: probe of 0-0010 failed with error -22

i2c-core: driver [isl29023] using legacy suspend method

i2c-core: driver [isl29023] using legacy resume method

snvs_rtc snvs_rtc.0: rtc core: registered snvs_rtc as rtc0

i2c /dev entries driver

Linux video capture interface: v2.00

pxp-v4l2 pxp-v4l2: initialized

i2c-core: driver [mag3110] using legacy suspend method

i2c-core: driver [mag3110] using legacy resume method

check mma8450 chip ID

mma8450 0-001c: read chip ID 0xfffffffb is not equal to 0xc6!

read chip ID failed

mma8450: probe of 0-001c failed with error -22

i2c-core: driver [mma8450] using legacy suspend method

i2c-core: driver [mma8450] using legacy resume method

add mma8450 i2c driver

imx2-wdt imx2-wdt.0: IMX2+ Watchdog Timer enabled. timeout=60s (nowayout=1)

Bluetooth: Virtual HCI driver ver 1.3

Bluetooth: HCI UART driver ver 2.2

Bluetooth: HCIATH3K protocol initialized

Bluetooth: Generic Bluetooth USB driver ver 0.6

usbcore: registered new interface driver btusb

sdhci: Secure Digital Host Controller Interface driver

sdhci: Copyright(c) Pierre Ossman

mmc0: SDHCI controller on platform [sdhci-esdhc-imx.0] using DMA

mmc1: SDHCI controller on platform [sdhci-esdhc-imx.1] using DMA

sdhci sdhci-esdhc-imx.2: no write-protect pin available!

mmc2: SDHCI controller on platform [sdhci-esdhc-imx.2] using DMA

Galcore version 4.6.9.6622

Thermal calibration data is 0x5674db69

Thermal sensor with ratio = 178

Anatop Thermal registered as thermal_zone0

anatop_thermal_probe: default cooling device is cpufreq!

dcp dcp.0: DCP crypto enabled.!

usbcore: registered new interface driver usbhid

usbhid: USB HID core driver

usbcore: registered new interface driver snd-usb-audio

mxc_spdif mxc_spdif.0: MXC SPDIF Audio

Cirrus Logic CS42888 ALSA SoC Codec Driver

i2c-core: driver [cs42888] using legacy suspend method

i2c-core: driver [cs42888] using legacy resume method

wm8962 1-001a: customer id 0 revision D

input: WM8962 Beep Generator as /devices/platform/imx-i2c.1/i2c-1/1-001a/input/input1

asoc: wm8962 <-> imx-ssi.1 mapping ok

input: wm8962-audio Ext Spk as /devices/platform/soc-audio.5/sound/card0/input2

imx_3stack asoc driver

asoc: mxc-spdif <-> imx-spdif-dai.0 mapping ok

Initialize HDMI-audio failed. Load HDMI-video first!

ALSA device list:

  #0: wm8962-audio

  #1: imx-spdif

TCP cubic registered

NET: Registered protocol family 17

can: controller area network core (rev 20090105 abi 8)

NET: Registered protocol family 29

can: raw protocol (rev 20090105)

can: broadcast manager protocol (rev 20090105 t)

Bluetooth: RFCOMM TTY layer initialized

Bluetooth: RFCOMM socket layer initialized

Bluetooth: RFCOMM ver 1.11

Bluetooth: BNEP (Ethernet Emulation) ver 1.3

Bluetooth: BNEP filters: protocol multicast

Bluetooth: HIDP (Human Interface Emulation) ver 1.2

lib80211: common routines for IEEE802.11 drivers

VFP support v0.3: implementor 41 architecture 3 part 30 variant 9 rev 4

Bus freq driver module loaded

Bus freq driver Enabled

mxc_dvfs_core_probe

DVFS driver module loaded

Thank you

0 件の賞賛
返信
4 返答(返信)

2,351件の閲覧回数
YixingKong
Senior Contributor IV

Sherrnidhi

This discussion is closed since no activity. If you still need help, please feel free to reply with an update to this discussion, or create another discussion.

Thanks,

Yixing

0 件の賞賛
返信

2,351件の閲覧回数
YixingKong
Senior Contributor IV

Shreenidhi

Had your issue got resolved? If yes, we are going to close the discussion in 3 days. If you still need help, please feel free to reply with an update to this discussion.

Thanks,

Yixing

0 件の賞賛
返信

2,351件の閲覧回数
AnsonHuang
NXP Employee
NXP Employee

We did NOT use hardware dvfs core for a long time, I don't think it is caused by DVFS. the whole log in my side is, so maybe you can try remove DVFS driver to have a try, need to pay attention to EPDC driver from below log:

Bluetooth: RFCOMM TTY layer initialized

Bluetooth: RFCOMM socket layer initialized

Bluetooth: RFCOMM ver 1.11

Bluetooth: BNEP (Ethernet Emulation) ver 1.3

Bluetooth: BNEP filters: protocol multicast

Bluetooth: HIDP (Human Interface Emulation) ver 1.2

lib80211: common routines for IEEE802.11 drivers

VFP support v0.3: implementor 41 architecture 3 part 30 variant 9 rev 4

Bus freq driver module loaded

Bus freq driver Enabled

mxc_dvfs_core_probe

DVFS driver module loaded

imx_epdc_fb imx_epdc_fb: Unable to get display PMIC regulator.err = 0xffffffed

regulator_init_complete: SPKVDD: incomplete constraints, leaving on

snvs_rtc snvs_rtc.0: setting system clock to 1970-01-01 00:00:00 UTC (0)

eth0: Freescale FEC PHY driver [Generic PHY] (mii_bus:phy_addr=1:00, irq=-1)

mmc1: new high speed SDHC card at address e024

mmcblk0: mmc1:e024 SD04G 3.69 GiB

mmcblk0: p1

PHY: 1:00 - Link is Up - 100/Full

0 件の賞賛
返信

2,351件の閲覧回数
alejandrolozan1
NXP Employee
NXP Employee

Hi,

Which images did you try?

Best Regards,

Alejandro

0 件の賞賛
返信