u-boot

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

u-boot

1,801 Views
saida
Contributor II

hi i.mx community

1. where i can see puts(),debug(),printf() defined source code and how it is working after seril_init() function ?

2. is there any hidden libraries in u-boot ?

3. where is dts file for sabresd dl board in u-boot ?

help in this regard

thank you

Labels (1)
Tags (1)
0 Kudos
Reply
2 Replies

1,717 Views
igorpadykov
NXP Employee
NXP Employee

Hi saida

for 1.2. one can post on uboot mail list:

U-Boot Info Page

regarding dts files, they are located in

linux_xxx/arch/arm/boot/dts/  folder

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,717 Views
saida
Contributor II

thank you igorpadykov

you are always helpful to me

i am happy with you reply

0 Kudos
Reply