u-boot support Camera/tv in display

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

u-boot support Camera/tv in display

跳至解决方案
2,379 次查看
zhanxiaozhang
Contributor III

Now in my project ,we have to do camera/tv in display in u-boot.

because I tried implement 'linux fast boot',it disable so many module ,maybe no sutiable our application.

Is there anyone have any solution or idea? thx!

0 项奖励
回复
1 解答
1,459 次查看
qiang_li-mpu_se
NXP Employee
NXP Employee

We don't have the uboot use case, but you can reference to the followee link: it is a small linux kernel mode to do the fast camera solution.

https://community.freescale.com/docs/DOC-93619

Test result of fast boot on Sabresd board for MIPI camera overly on LVDS screen:

     The main application be executed from the board be powered up is about 958ms.

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,460 次查看
qiang_li-mpu_se
NXP Employee
NXP Employee

We don't have the uboot use case, but you can reference to the followee link: it is a small linux kernel mode to do the fast camera solution.

https://community.freescale.com/docs/DOC-93619

Test result of fast boot on Sabresd board for MIPI camera overly on LVDS screen:

     The main application be executed from the board be powered up is about 958ms.

0 项奖励
回复