u-boot support Camera/tv in display

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

u-boot support Camera/tv in display

Jump to solution
2,380 Views
zhanxiaozhang
Contributor III

Now in my project ,we have to do camera/tv in display in u-boot.

because I tried implement 'linux fast boot',it disable so many module ,maybe no sutiable our application.

Is there anyone have any solution or idea? thx!

0 Kudos
Reply
1 Solution
1,460 Views
qiang_li-mpu_se
NXP Employee
NXP Employee

We don't have the uboot use case, but you can reference to the followee link: it is a small linux kernel mode to do the fast camera solution.

https://community.freescale.com/docs/DOC-93619

Test result of fast boot on Sabresd board for MIPI camera overly on LVDS screen:

     The main application be executed from the board be powered up is about 958ms.

View solution in original post

0 Kudos
Reply
1 Reply
1,461 Views
qiang_li-mpu_se
NXP Employee
NXP Employee

We don't have the uboot use case, but you can reference to the followee link: it is a small linux kernel mode to do the fast camera solution.

https://community.freescale.com/docs/DOC-93619

Test result of fast boot on Sabresd board for MIPI camera overly on LVDS screen:

     The main application be executed from the board be powered up is about 958ms.

0 Kudos
Reply