u-boot support Camera/tv in display

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

u-boot support Camera/tv in display

ソリューションへジャンプ
3,051件の閲覧回数
zhanxiaozhang
Contributor III

Now in my project ,we have to do camera/tv in display in u-boot.

because I tried implement 'linux fast boot',it disable so many module ,maybe no sutiable our application.

Is there anyone have any solution or idea? thx!

0 件の賞賛
返信
1 解決策
2,131件の閲覧回数
qiang_li-mpu_se
NXP Employee
NXP Employee

We don't have the uboot use case, but you can reference to the followee link: it is a small linux kernel mode to do the fast camera solution.

https://community.freescale.com/docs/DOC-93619

Test result of fast boot on Sabresd board for MIPI camera overly on LVDS screen:

     The main application be executed from the board be powered up is about 958ms.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,132件の閲覧回数
qiang_li-mpu_se
NXP Employee
NXP Employee

We don't have the uboot use case, but you can reference to the followee link: it is a small linux kernel mode to do the fast camera solution.

https://community.freescale.com/docs/DOC-93619

Test result of fast boot on Sabresd board for MIPI camera overly on LVDS screen:

     The main application be executed from the board be powered up is about 958ms.

0 件の賞賛
返信