u-boot.imx does not have DCD ptr & Boot Data Ptr ( imximage.cfg is missing)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

u-boot.imx does not have DCD ptr & Boot Data Ptr ( imximage.cfg is missing)

1,623 Views
kanimozhi_t
Contributor V

Hello,

     I'm following the Freescale's U-boot repo( GitHub - Freescale/u-boot-fslc: U-Boot tree to host pending fixes and improvements ) for building secure boot in i.MX 6UL EVK (14 X 14). I'm stuck in the stage of building u-boot.imx.

The command I use is

make u-boot.imx

The generated imx file has both DCD ptr & Boot data ptr as 0 (zero). After some searching I found that the imximage.cfg is missing from /board/freescale/mx6ul_14x14_evk/

So, it'll be very helpful if someone could refer which file to locate or how to generate imximage.cfg for the i.MX 6UL EVK.

Thanks in advance!

Labels (2)
1 Reply

1,507 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello Kanimozhi Thangappan,

The uboot you are referring to is the Community BSP uboot. There are several branches and it’s supported by the community, although this repository has not been updated for a while.

If possible, I would recommend the BSP release repositories, although they cover only NXP boards (which in this case should be no problem)

http://git.freescale.com/git/cgit.cgi/imx/uboot-imx.git/

I hope this helps!

Regards,