u-boot error: No partition table - mmc 2 Couldn't find partition mmc 2:1

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

u-boot error: No partition table - mmc 2 Couldn't find partition mmc 2:1

1,397 Views
vprajapati
Contributor II

I am working on imx8mp custom board which has 2 GB DDR4 RAM. It has 64 GB of emmc. I am flashing yocto images which has Kernel 6.6.23 and U-Boot 2024.04

First time I made some customization and flashed that image, it is working well. Then 2nd time, made some customization and added some debug logs in kernel and u-boot. The image stopped working and each time stucks in u-boot console. Even the first image that was working previously, it is not working now. 

The u-boot logs with environment is showing below.

 

 

U-Boot 2024.04+g674440bc73e+p0 (Jun 06 2024 - 10:05:34 +0000)

CPU:   i.MX8MP[8] rev1.1 1600 MHz (running at 1200 MHz)
CPU:   Industrial temperature grade (-40C to 105C) at 39C
Reset cause: POR
Model: Invixium Access i.MX8MPlus DDR4 Eco Face board
DRAM:  2 GiB
Core:  101 devices, 26 uclasses, devicetree: separate
NAND:  0 MiB
MMC:   FSL_SDHC: 1, FSL_SDHC: 2
Loading Environment from MMC... *** Warning - bad CRC, using default environment

[*]-Video Link 0fail to get display timings
probe video device failed, ret -22

        [0] lcd-controller@32e80000, video
        [1] mipi_dsi@32e60000, video_bridge
fail to get display timings
probe video device failed, ret -22
In:    serial
Out:   serial
Err:   serial
SEC0:  RNG instantiated
switch to partitions #0, OK
mmc2(part 0) is current device
flash target is MMC:2
Net:   
Error: ethernet@30bf0000 No valid MAC address found.
No ethernet found.

Fastboot: Normal
Normal Boot
Hit any key to stop autoboot:  0 
starting USB...
Bus usb@38200000: Register 2000140 NbrPorts 2
Starting the controller
USB XHCI 1.10
scanning bus usb@38200000 for devices... 1 USB Device(s) found
       scanning usb for storage devices... 0 Storage Device(s) found

Device 0: unknown device
MMC: no card present
switch to partitions #0, OK
mmc2(part 0) is current device
** No partition table - mmc 2 **
Couldn't find partition mmc 2:1
Running BSP bootcmd ...
switch to partitions #0, OK
mmc2(part 0) is current device
** No partition table - mmc 2 **
Couldn't find partition mmc 2:1
Can't set block device
** No partition table - mmc 2 **
Couldn't find partition mmc 2:1
Can't set block device
Booting from net ...

Error: ethernet@30bf0000 No valid MAC address found.

Error: ethernet@30bf0000 No valid MAC address found.

Error: ethernet@30bf0000 No valid MAC address found.

Error: ethernet@30bf0000 No valid MAC address found.
No ethernet found.

Error: ethernet@30bf0000 No valid MAC address found.

Error: ethernet@30bf0000 No valid MAC address found.

Error: ethernet@30bf0000 No valid MAC address found.

Error: ethernet@30bf0000 No valid MAC address found.

Error: ethernet@30bf0000 No valid MAC address found.
No ethernet found.

Error: ethernet@30bf0000 No valid MAC address found.
WARN: Cannot load the DT
u-boot-ecoface=> mmc info
Device: FSL_SDHC
Manufacturer ID: 70
OEM: 0
Name: TY2964 
Bus Speed: 200000000
Mode: HS400ES (200MHz)
Rd Block Len: 512
MMC version 5.1
High Capacity: Yes
Capacity: 58.3 GiB
Bus Width: 8-bit DDR
Erase Group Size: 512 KiB
HC WP Group Size: 8 MiB
User Capacity: 58.3 GiB
Boot Capacity: 4 MiB ENH
RPMB Capacity: 4 MiB ENH
Boot area 0 is not write protected
Boot area 1 is not write protected
u-boot-ecoface=> 
u-boot-ecoface=> printenv
arch=arm
baudrate=115200
board=imx8mp_evk
board_name=IXM-ECOFACE
board_rev=ECOFACE_1_0
boot_a_script=load ${devtype} ${devnum}:${distro_bootpart} ${scriptaddr} ${prefix}${script}; source ${scriptaddr}
boot_efi_binary=load ${devtype} ${devnum}:${distro_bootpart} ${kernel_addr_r} efi/boot/bootaa64.efi; if fdt addr -q ${fdt_addr_r}; then bootefi ${kernel_addr_r} ${fdt_addr_r};else bootefi ${kernel_addr_i
boot_efi_bootmgr=if fdt addr -q ${fdt_addr_r}; then bootefi bootmgr ${fdt_addr_r};else bootefi bootmgr;fi
boot_extlinux=sysboot ${devtype} ${devnum}:${distro_bootpart} any ${scriptaddr} ${prefix}${boot_syslinux_conf}
boot_fdt=try
boot_fit=no
boot_net_usb_start=usb start
boot_prefixes=/ /boot/
boot_script_dhcp=boot.scr.uimg
boot_scripts=boot.scr.uimg boot.scr
boot_syslinux_conf=extlinux/extlinux.conf
boot_targets=usb0 mmc1 mmc2 
bootargs=console=ttymxc1,115200 root=/dev/nfs ip=dhcp nfsroot=:,v3,tcp
bootcmd=run distro_bootcmd;run bsp_bootcmd
bootcmd_mfg=run mfgtool_args;if iminfo ${initrd_addr}; then if test ${tee} = yes; then bootm ${tee_addr} ${initrd_addr} ${fdt_addr}; else booti ${loadaddr} ${initrd_addr} ${fdt_addr}; fi; else echo "Run;
bootcmd_mmc1=devnum=1; run mmc_boot
bootcmd_mmc2=devnum=2; run mmc_boot
bootcmd_usb0=devnum=0; run usb_boot
bootdelay=2
bootm_size=0x10000000
bootscript=echo Running bootscript from mmc ...; source
bsp_bootcmd=echo Running BSP bootcmd ...; mmc dev ${mmcdev}; if mmc rescan; then if run loadbootscript; then run bootscript; else if run loadimage; then run mmcboot; else run netboot; fi; fi; fi;
bsp_script=boot.scr
console=ttymxc1,115200
cpu=armv8
distro_bootcmd=for target in ${boot_targets}; do run bootcmd_${target}; done
efi_dtb_prefixes=/ /dtb/ /dtb/current/
emmc_dev=2
fastboot_dev=mmc2
fdt_addr=0x43000000
fdt_addr_r=0x43000000
fdt_high=0xffffffffffffffff
fdtcontroladdr=bced5e40
fdtfile=ixm-ecoface.dtb
get_cmd=dhcp
image=Image
initrd_addr=0x43800000
initrd_high=0xffffffffffffffff
jh_clk= 
jh_mmcboot=setenv fdtfile ${jh_root_dtb};setenv jh_clk clk_ignore_unused mem=1920MB; if run loadimage; then run mmcboot; else run jh_netboot; fi; 
jh_netboot=setenv fdtfile ${jh_root_dtb}; setenv jh_clk clk_ignore_unused mem=1920MB; run netboot; 
jh_root_dtb=imx8mp-evk-root.dtb
kboot=booti 
kernel_addr_r=0x40400000
load_efi_dtb=load ${devtype} ${devnum}:${distro_bootpart} ${fdt_addr_r} ${prefix}${efi_fdtfile}
loadaddr=0x40400000
loadbootscript=fatload mmc ${mmcdev}:${mmcpart} ${loadaddr} ${bsp_script};
loadfdt=fatload mmc ${mmcdev}:${mmcpart} ${fdt_addr_r} ${fdtfile}
loadimage=fatload mmc ${mmcdev}:${mmcpart} ${loadaddr} ${image}
mfgtool_args=setenv bootargs console=${console},${baudrate} rdinit=/linuxrc clk_ignore_unused 
mmc_boot=if mmc dev ${devnum}; then devtype=mmc; run scan_dev_for_boot_part; fi
mmcargs=setenv bootargs ${jh_clk} ${mcore_clk} console=${console} root=${mmcroot}
mmcautodetect=yes
mmcboot=echo Booting from mmc ...; run mmcargs; if test ${boot_fit} = yes || test ${boot_fit} = try; then bootm ${loadaddr}; else if run loadfdt; then booti ${loadaddr} - ${fdt_addr_r}; else echo WARN: ;
mmcdev=2
mmcpart=1
mmcroot=/dev/mmcblk2p2 rootwait rw
mtdids=nand0=gpmi-nand
nandfit_part=yes
netargs=setenv bootargs ${jh_clk} ${mcore_clk} console=${console} root=/dev/nfs ip=dhcp nfsroot=${serverip}:${nfsroot},v3,tcp
netboot=echo Booting from net ...; run netargs;  if test ${ip_dyn} = yes; then setenv get_cmd dhcp; else setenv get_cmd tftp; fi; ${get_cmd} ${loadaddr} ${image}; if test ${boot_fit} = yes || test ${boo;
nodes=/busfreq /power-domains /soc@0/caam-sm@100000 /soc@0/bus@30000000/caam_secvio /soc@0/bus@30000000/caam-snvs@30370000 /soc@0/bus@30800000/flexspi_nand@30bb0000 /soc@0/bus@32c00000/mipi_dsi@32e60000 
prepare_mcore=setenv mcore_clk clk-imx8mp.mcore_booted;
scan_dev_for_boot=echo Scanning ${devtype} ${devnum}:${distro_bootpart}...; for prefix in ${boot_prefixes}; do run scan_dev_for_extlinux; run scan_dev_for_scripts; done;run scan_dev_for_efi;
scan_dev_for_boot_part=part list ${devtype} ${devnum} -bootable devplist; env exists devplist || setenv devplist 1; for distro_bootpart in ${devplist}; do if fstype ${devtype} ${devnum}:${distro_bootpart
scan_dev_for_efi=setenv efi_fdtfile ${fdtfile}; for prefix in ${efi_dtb_prefixes}; do if test -e ${devtype} ${devnum}:${distro_bootpart} ${prefix}${efi_fdtfile}; then run load_efi_dtb; fi;done;run boot_e
scan_dev_for_extlinux=if test -e ${devtype} ${devnum}:${distro_bootpart} ${prefix}${boot_syslinux_conf}; then echo Found ${prefix}${boot_syslinux_conf}; run boot_extlinux; echo EXTLINUX FAILED: continuii
scan_dev_for_scripts=for script in ${boot_scripts}; do if test -e ${devtype} ${devnum}:${distro_bootpart} ${prefix}${script}; then echo Found U-Boot script ${prefix}${script}; run boot_a_script; echo SCe
scriptaddr=0x43500000
sd_dev=1
serial#=090c1800596878c0
soc=imx8m
soc_type=imx8mp
splashimage=0x50000000
sr_ir_v2_cmd=cp.b ${fdtcontroladdr} ${fdt_addr_r} 0x10000;fdt addr ${fdt_addr_r};fdt set /soc@0/usb@32f10100/usb@38100000 compatible snps,dwc3;fdt set /soc@0/usb@32f10108/usb@38200000 compatible snps,dw 
ubifs_boot=if ubi part ${bootubipart} ${bootubioff} && ubifsmount ubi0:${bootubivol}; then devtype=ubi; devnum=ubi0; bootfstype=ubifs; distro_bootpart=${bootubivol}; run scan_dev_for_boot; ubifsumount; i
usb_boot=usb start; if usb dev ${devnum}; then devtype=usb; run scan_dev_for_boot_part; fi
vendor=freescale

Environment size: 6521/16380 bytes
u-boot-ecoface=> 

 

 

I try to erase emmc and re flashed the image, still the same problem.  What should be the issue here any detailed debugging steps would help me.

I am flashing wic.zst image created by yocto using uuu utility using below command
uuu -b emmc_all imx-boot-ixm-ecoface-sd.bin-flash_ddr4_evk ixm-ecoface-image-ixm-ecoface.rootfs.wic.zst

I am attaching my board def config file, dtsi files and .c and .h files for board.

Thanks.



0 Kudos
Reply
0 Replies