u-boot does not boot from emmc

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

u-boot does not boot from emmc

3,092件の閲覧回数
niharunadkat
Contributor I

Hi,

 

I am trying to boot from an emmc and this is the error message i get when my ARM units boots

 

U-Boot SPL 2017.11 (Jul 31 2019 - 11:45:24)                                     
Initializing DDR....using SPD                                                   
Trying to boot from MMC1                                                        
mmc_init: -110, time 43                                                         
spl: mmc init failed with error: -110                                           
SPL: failed to boot from all boot devices                                       
### ERROR ### Please RESET the board ###

 

I can use the same u-boot-with-spl-pbl.bin and boot from and SD card. What i am missing?

 

Please provide any information for the issue seen# above.

 

Thank you

Nihar

0 件の賞賛
返信
2 返答(返信)

2,702件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

The images download to SD and EMMC are the same, only the boot modes are different.

0 件の賞賛
返信

2,702件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

Which board and which version of BSP are you using?

0 件の賞賛
返信