u-boot args with hdmi

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

u-boot args with hdmi

Jump to solution
2,277 Views
jiejia
Contributor III

while  bootargs=console=ttymxc0,115200 video=mxcfb0:dev=hdmi,1920x1080M@60,if=RGB24,bpp=32,    the egl/gles display well.

while bootargs=console=ttymxc0,115200 video=mxcfb0:dev=hdmi,1920x1080M@60,if=RGB24,bpp=24,    the egl/gles display error.

Why can't I set the bpp=24 while if=RGB24?

Labels (1)
0 Kudos
Reply
1 Solution
2,012 Views
igorpadykov
NXP Employee
NXP Employee

Hi jie

please refer to attached MX_6_Graphics_User's_Guide

sect.6.1.2 24 bpp pixmap :

The GPU can only accelerate a 16 bpp or 32 bpp pixmap.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
2,013 Views
igorpadykov
NXP Employee
NXP Employee

Hi jie

please refer to attached MX_6_Graphics_User's_Guide

sect.6.1.2 24 bpp pixmap :

The GPU can only accelerate a 16 bpp or 32 bpp pixmap.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply