u-Boot changing ethernet speed with i.MX6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

u-Boot changing ethernet speed with i.MX6

Jump to solution
4,488 Views
_Anthony
Contributor II
Hello,
 
I hope you're going well in this period,
 
I permit to contact you because I've got a question about how to change the ethernet connection flow from 100 to 1000 Mb/s in u-boot environment.
 
So Actually, I know the following commands permit to limit connexion flow to 100 Mb/s:
 
=> mdio write FEC 9 0
=> mdio write FEC 0 3300
 
But I would like to reverse the operation to limit connexion flow to 1000Mb/s.
 
The mmi dump command shows we're in 100Mb/s.
 
=> mii dump          
0.     (3100)                 -- PHY control register --
  (8000:0000) 0.15    =     0    reset
  (4000:0000) 0.14    =     0    loopback
  (2040:2000) 0. 6,13 =   b01    speed selection = 100 Mbps
  (1000:1000) 0.12    =     1    A/N enable
  (0800:0000) 0.11    =     0    power-down
  (0400:0000) 0.10    =     0    isolate
  (0200:0000) 0. 9    =     0    restart A/N
  (0100:0100) 0. 8    =     1    duplex = full
  (0080:0000) 0. 7    =     0    collision test enable
  (003f:0000) 0. 5- 0 =     0    (reserved)
 
 
Do you know how can I switch to 1000Mb/s mode? What are the mdio FEC commands?
 
Thanks for all and best reguards.
 

Anthony.

0 Kudos
Reply
1 Solution
4,483 Views
igorpadykov
NXP Employee
NXP Employee

Hi Anthony

 

one can try to set bits 6,13 = b10 speed selection = 1000 Mbps
/* Basic mode control register. */
#define BMCR_SPEED1000 0x0040 /* MSB of Speed (1000)
#define BMCR_SPEED100 0x2000 /* Select 100Mbps 

https://source.codeaurora.org/external/imx/uboot-imx/tree/include/linux/mii.h?h=imx_v2020.04_5.4.70_...

 

Best regards
igor

View solution in original post

0 Kudos
Reply
2 Replies
4,484 Views
igorpadykov
NXP Employee
NXP Employee

Hi Anthony

 

one can try to set bits 6,13 = b10 speed selection = 1000 Mbps
/* Basic mode control register. */
#define BMCR_SPEED1000 0x0040 /* MSB of Speed (1000)
#define BMCR_SPEED100 0x2000 /* Select 100Mbps 

https://source.codeaurora.org/external/imx/uboot-imx/tree/include/linux/mii.h?h=imx_v2020.04_5.4.70_...

 

Best regards
igor

0 Kudos
Reply
4,474 Views
_Anthony
Contributor II

Hello,

Thanks for your response.

So I success to do it with theses commands:

mdio write FEC 9 300

mdio write FEC 0 1340

Best reguards.

0 Kudos
Reply