ts_calibrate issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

ts_calibrate issue

4,119件の閲覧回数
wangvictor
Contributor III

Hi All,

I'm using i.MX6 sabresd for my layer.

And I'm using egalax resist touch so I need to using ts_calibrate to reconfigure my touch xres and yres.

Now I am facing the problem that my xres and yres are opposite.

How to fix this problem?

Thanks in Advanced!

ラベル(6)
0 件の賞賛
返信
6 返答(返信)

3,911件の閲覧回数
wangvictor
Contributor III

igorpadykov 員工

I've check that hardware is correct.(By using other OS system)

In console touch works perfectly by using ts_test but when I get in to wayland weston it will be wrong.

I think it is the issue of qtwayland.

I don't know what should I set in wayland.

Any suggestion?

Thanks in Advanced!

0 件の賞賛
返信

3,911件の閲覧回数
wangvictor
Contributor III

igorpadykov 員工

Sorry for asking, why is this problem relative to hardware issue?

I thought the X and Y value is correct.

 Thanks in Advanced!

0 件の賞賛
返信

3,911件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

because you said "xres and yres are opposite".

Had you tried to debug it and compare with good board.

Best regards
igor

0 件の賞賛
返信

3,911件の閲覧回数
wangvictor
Contributor III

@igorpadykov

This is what I got when I run ts_calibrate.

I pointed five place and this is the value I got.

Took 2 samples...
Top left : X = 1912 Y = 1825
Took 1 samples...
Top right : X = 140 Y = 1818
Took 3 samples...
Bot right : X = 147 Y = 206
Took 2 samples...
Bot left : X = 1926 Y = 234
Took 1 samples...
Center : X = 1049 Y = 1066
1053.816406 -0.520339 -0.003272
618.019897 0.003143 -0.311976
Calibration constants: 69062912 -34100 -214 40502552 205 -20445 65536

But after I finished calibrate it still got the issue like this.

I click the place where locate at panel's right _top corner -> pointer will go left_down

I click the place where locate at panel's right _down corner-> pointer will go left_top

In the other hand, I tried to using ts_test to draw a line, it works perfectly.

How to fix this problem?

Thanks in Advanced!

0 件の賞賛
返信

3,911件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Wang

please recheck touch hardware and schematic, to exclude connection issue.

Best regards
igor

0 件の賞賛
返信

3,911件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Wang

one can look at driver sources an debug it

linux-imx6/egalax_ts.c at boundary-imx_3.0.35_1.1.1 · boundarydevices/linux-imx6 · GitHub 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信