tinycap command cannot be recorded

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

tinycap command cannot be recorded

3,887 Views
yzg
Contributor I

Now I have a problem. After tinymix is used to set the recording quality to high mode, the recording will be interrupted this time. The next time tinycap command is used to record the recording, 100% cannot be recorded, there will be no error message, but the recorded audio is empty.If the recording quality setting layer is in low mode, this problem does not exist

0 Kudos
Reply
4 Replies

3,853 Views
Harvey021
NXP TechSupport
NXP TechSupport

Hi 

Are you using evk board or other board? and what codec?

Can you share the procedures of full commands? 

 

Best regards

Harvey

0 Kudos
Reply

3,845 Views
yzg
Contributor I

1,codec is kernel_imx/sound/soc/fsl/fsl_micfil.c

2,board is not evk, it is another board

3,full command:

tinycap test.wav -D 1-d 0-c 2-r 48000-b 16 (Recording works properly)

tinymix -D 1 8 1

tinycap test.wav -D 1 -d 0 -c 2 -r 48000 -b 16 (Failed to record)

0 Kudos
Reply

3,859 Views
Harvey021
NXP TechSupport
NXP TechSupport

Hi @yzg 

Is the sound play okay with the current device?

By the way, let me know which BSP and device you are working with.

And can you share the logcat?

 

Best regards

Harvey

 

 

Best regards

Harvey

 

0 Kudos
Reply

3,857 Views
yzg
Contributor I

Hi

Thank you for your reply. I use the imx8mm processor and the Linux version is 4.14.98.Sound can be played correctly

0 Kudos
Reply