the prebuilt u-boot image for MCIMX6Q-SDB C6

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

the prebuilt u-boot image for MCIMX6Q-SDB C6

1,175 次查看
liamtien
Contributor I

I am using “MCIMX6Q-SDB”, its version is  C6, bought from DigiKey. So far, I only install SPL and u-boot.img to SD card follow the eewiki.net instructions(below is the website) but it has no message output in serial console. 

   i.MX6q SABRE Board for Smart Devices - Linux on ARM - eewiki 
    I wonder something or step is missing, does anyone has the prebuilt u-boot image and related files for C6 board? I'd like to try it. Thanks!

标签 (1)
0 项奖励
回复
1 回复

1,010 次查看
gusarambula
NXP TechSupport
NXP TechSupport

Hello liam Tien,

I haven’t tested the images available on the eeWiki, but these should be similar to the NXP BSP.

My recommendation would be using the images available as part of the NXP BSP or contacting the authors from the eeWiki for more information on their documentation.

You can download the i.MX6Q SABRE SDB images and documentation on the following links (please note that you may need to login to download this files).

 

L4.1.15_2.0.0 Linux Documentation
https://www.nxp.com/webapp/Download?colCode=L4.1.15_2.0.0-LINUX-DOCS&Parent_nodeId=14640214319777009...

 

L4.1.15_2.0.0 Linux BSP Images
https://www.nxp.com/webapp/Download?colCode=L4.1.15_2.0.0_MX6QDLSOLO&appType=license&Parent_nodeId=1...

I hope this helps!

Regards,

0 项奖励
回复