tft lcd

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

tft lcd

3,184件の閲覧回数
vahidnoori
Contributor II

i have a imx5 and imx6 board . i decided to run tft lcd by its. but i dont know what tft is suitable (lvds interface and driver for linux) for this boards???

ラベル(4)
0 件の賞賛
返信
5 返答(返信)

2,801件の閲覧回数
weidong_sun
NXP TechSupport
NXP TechSupport

Hello,vahid,

     (1) i.mx51

          there are 2 parallel LCD interfaces on i.mx51, both support RGB24 , RGB666, RGB565.

     (2)i.mx53

         there are 2 LVDS ports(LVDS0 and LVDS1) and 2 parallel ports(DISP0 and DISP1, normally, we use DISP0)

     (3)I.MX6

         We have I.MX6SL, i.mx6s/dl/d/q, I.MX6SL is designed for E-book. i.mx6sl/dl/dq can be designed all-in-one board. they also support  2 LVDS ports(LVDS0 and LVDS1) and 2 parallel ports(DISP0 and DISP1, normally, we use DISP0).

Mode details, you can download their schematic from our website, you will find those interface I metioned above.

   As for driver of LCD you will use, you should porting it to linux or android system according to your LCD spec, it is not difficult , you only need to add your LCD timing to our bsp.

Regards,

weidong

0 件の賞賛
返信

2,801件の閲覧回数
vahidnoori
Contributor II

Hello.

Ye I know it but I don't know which tft lcd that has both lvds and driver of linux is suitable for imx53

Sent from my HTC

0 件の賞賛
返信

2,801件の閲覧回数
Yuri
NXP Employee
NXP Employee

The i.MX53 BSP(s) suport CLAA WVGA and Seiko WVGA panels.

It was tested with i.MX53 START-R design.

Also HannStar LVDS panel is supported by BSPs.

0 件の賞賛
返信

2,801件の閲覧回数
vahidnoori
Contributor II

hello.

is each lcd that has LVDS interface supported and matched by imx53?if no

which on of LCD that has LVDS is suitable for imx53?

On Wed, Nov 13, 2013 at 10:24 AM, Yuri Muhin

0 件の賞賛
返信

2,801件の閲覧回数
EgleTeam
Contributor V

LVDS is only the physical layer: parallel RGB serialized. Almost any LVDS display should work with iMX6/iMX5 (provided no extra config by I2C be necessary). We've tried some displays recycled from old laptops and they worked perfect.

Good luck!

0 件の賞賛
返信