tflite_runtime + NNAPI stops working when a computational heavy thread is started

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

tflite_runtime + NNAPI stops working when a computational heavy thread is started

4,494件の閲覧回数
FSet89
Contributor I

I am working on a script that is deployed on a IMX8MP with NPU and NNAPI. The script makes inferences using the tflite_runtime library. If a thread is started producing a high cpu usage, tflite stops working, producing always the same result regardless of the input. I provided a minimum working example on github. The problem is not encountered on my PC. Is it related to NNAPI?

ラベル(1)
0 件の賞賛
返信
8 返答(返信)

4,474件の閲覧回数
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hi @FSet89 

Can you share your test script ,model and steps?

0 件の賞賛
返信

4,446件の閲覧回数
FSet89
Contributor I

Hi, I tried to share the code but my reply keeps getting deleted. However you can find the code in the linked github issue. I cannot share the model but you can try with any quantized tflite model.

0 件の賞賛
返信

4,388件の閲覧回数
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Please try the vx_delegate not NNAPI. The NNAPI is not maintained by NXP

 delegate = tflite.load_delegate('/usr/lib/libvx_delegate.so')
 self.interpreter = tflite.Interpreter(model_path=path, experimental_delegates=[delegate])
0 件の賞賛
返信

4,369件の閲覧回数
FSet89
Contributor I

Thank you for your suggestion. I don't have the vx_delegate in my Yocto system. Can you provide me some reference about how to add it to Yocto?

0 件の賞賛
返信

4,346件の閲覧回数
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hi @FSet89 

You can refer the i.MX Yocto Project User’s Guide​ to dowlnad i.MX yocto project from this website https://www.nxp.com/design/software/embedded-software/i-mx-software/embedded-linux-for-i-mx-applicat...

Then copy the layer /sources/meta-imx/meta-ml/ to your Yocto project.

0 件の賞賛
返信

3,974件の閲覧回数
FSet89
Contributor I

Hi @Zhiming_Liu , I already have this layer but I don't have /usr/lib/libvx_delegate.so in my compiled system. Should I edit my recipe?

0 件の賞賛
返信

4,435件の閲覧回数
FSet89
Contributor I

Hi @Zhiming_Liu , here is the code. I cannot share the model but you can try with any quantized tflite model:

 

import multiprocessing
from multiprocessing import Queue, Process
import numpy as np
from threading import Thread
from random import random, randint
import tflite_runtime.interpreter as tflite
import time
import cv2 
import os
import sys
import psutil

class ClassificationModel(object):
	def __init__(self, path, mask_path=None):
		self.interpreter = tflite.Interpreter(model_path=path)
		self.interpreter.allocate_tensors()
		self.input_details = self.interpreter.get_input_details()
		self.output_details = self.interpreter.get_output_details()
		self.input_shape = self.input_details[0]['shape']



	def predict(self, img, resize=True):

		if resize:
			img = cv2.resize(img, (self.input_shape[2], self.input_shape[1]))		

		img = (img/255.0).astype(np.float32)
		img = np.expand_dims(img, 0)
		self.interpreter.set_tensor(self.input_details[0]['index'], img)				
		self.interpreter.invoke()			
		output = self.interpreter.get_tensor(self.output_details[0]['index'])
		output = np.squeeze(output)
		
		return output



def my_thread_1():
	print("Start threaded task 1")
	simulate_cpu_load()

	print("Task 1 completed")


def worker():
	while True:
		pass

def simulate_cpu_load():
	num_cores = multiprocessing.cpu_count()
	processes = []

	for _ in range(num_cores):
		p = multiprocessing.Process(target=worker)
		p.start()
		processes.append(p)

	time.sleep(3) 

	for p in processes:
		p.terminate()




if __name__ == '__main__':
	classifier_1 = ClassificationModel('mymodel.tflite)	
	
	cap = cv2.VideoCapture()
	for i in range(5):
		cap.open(i)
		if cap.isOpened():
			break

	if not cap.isOpened():
		print("Could not open camera")
		exit()


	try:
		while True:		
			# get image			
			ret, img = cap.read()

			# predict			
			p1 = classifier_1.predict(img)
			print(p1)			

			# threaded task
			if random() < 0.1:
				t = Thread(target=my_thread_1)
				t.start()
			
	except(KeyboardInterrupt):
		exit()  

 

0 件の賞賛
返信

4,314件の閲覧回数
FSet89
Contributor I

Hi, here is the code. I cannot share the model but you can try with any quantized tflite model.

 

import multiprocessing
from multiprocessing import Queue, Process
import numpy as np
from threading import Thread
from random import random, randint
import tflite_runtime.interpreter as tflite
import time
import cv2 
import os
import sys
import psutil

class ClassificationModel(object):
	def __init__(self, path, mask_path=None):
		self.interpreter = tflite.Interpreter(model_path=path)
		self.interpreter.allocate_tensors()
		self.input_details = self.interpreter.get_input_details()
		self.output_details = self.interpreter.get_output_details()
		self.input_shape = self.input_details[0]['shape']



	def predict(self, img, resize=True):

		if resize:
			img = cv2.resize(img, (self.input_shape[2], self.input_shape[1]))		

		img = (img/255.0).astype(np.float32)
		img = np.expand_dims(img, 0)
		self.interpreter.set_tensor(self.input_details[0]['index'], img)				
		self.interpreter.invoke()			
		output = self.interpreter.get_tensor(self.output_details[0]['index'])
		output = np.squeeze(output)
		
		return output



def my_thread_1():
	print("Start threaded task 1")
	simulate_cpu_load()

	print("Task 1 completed")


def worker():
	while True:
		pass

def simulate_cpu_load():
	num_cores = multiprocessing.cpu_count()
	processes = []

	for _ in range(num_cores):
		p = multiprocessing.Process(target=worker)
		p.start()
		processes.append(p)

	time.sleep(3) 

	for p in processes:
		p.terminate()




if __name__ == '__main__':
	classifier_1 = ClassificationModel('mymodel.tflite)	
	
	cap = cv2.VideoCapture()
	for i in range(5):
		cap.open(i)
		if cap.isOpened():
			break

	if not cap.isOpened():
		print("Could not open camera")
		exit()


	try:
		while True:		
			# get image			
			ret, img = cap.read()

			# predict			
			p1 = classifier_1.predict(img)
			print(p1)			

			# threaded task
			if random() < 0.1:
				t = Thread(target=my_thread_1)
				t.start()
			
	except(KeyboardInterrupt):
		exit()
0 件の賞賛
返信