tflite_runtime + NNAPI stops working when a computational heavy thread is started

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

tflite_runtime + NNAPI stops working when a computational heavy thread is started

2,527 次查看
FSet89
Contributor I

I am working on a script that is deployed on a IMX8MP with NPU and NNAPI. The script makes inferences using the tflite_runtime library. If a thread is started producing a high cpu usage, tflite stops working, producing always the same result regardless of the input. I provided a minimum working example on github. The problem is not encountered on my PC. Is it related to NNAPI?

标签 (1)
0 项奖励
回复
8 回复数

2,507 次查看
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hi @FSet89 

Can you share your test script ,model and steps?

0 项奖励
回复

2,479 次查看
FSet89
Contributor I

Hi, I tried to share the code but my reply keeps getting deleted. However you can find the code in the linked github issue. I cannot share the model but you can try with any quantized tflite model.

0 项奖励
回复

2,421 次查看
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Please try the vx_delegate not NNAPI. The NNAPI is not maintained by NXP

 delegate = tflite.load_delegate('/usr/lib/libvx_delegate.so')
 self.interpreter = tflite.Interpreter(model_path=path, experimental_delegates=[delegate])
0 项奖励
回复

2,402 次查看
FSet89
Contributor I

Thank you for your suggestion. I don't have the vx_delegate in my Yocto system. Can you provide me some reference about how to add it to Yocto?

0 项奖励
回复

2,379 次查看
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hi @FSet89 

You can refer the i.MX Yocto Project User’s Guide​ to dowlnad i.MX yocto project from this website https://www.nxp.com/design/software/embedded-software/i-mx-software/embedded-linux-for-i-mx-applicat...

Then copy the layer /sources/meta-imx/meta-ml/ to your Yocto project.

0 项奖励
回复

2,007 次查看
FSet89
Contributor I

Hi @Zhiming_Liu , I already have this layer but I don't have /usr/lib/libvx_delegate.so in my compiled system. Should I edit my recipe?

0 项奖励
回复

2,468 次查看
FSet89
Contributor I

Hi @Zhiming_Liu , here is the code. I cannot share the model but you can try with any quantized tflite model:

 

import multiprocessing
from multiprocessing import Queue, Process
import numpy as np
from threading import Thread
from random import random, randint
import tflite_runtime.interpreter as tflite
import time
import cv2 
import os
import sys
import psutil

class ClassificationModel(object):
	def __init__(self, path, mask_path=None):
		self.interpreter = tflite.Interpreter(model_path=path)
		self.interpreter.allocate_tensors()
		self.input_details = self.interpreter.get_input_details()
		self.output_details = self.interpreter.get_output_details()
		self.input_shape = self.input_details[0]['shape']



	def predict(self, img, resize=True):

		if resize:
			img = cv2.resize(img, (self.input_shape[2], self.input_shape[1]))		

		img = (img/255.0).astype(np.float32)
		img = np.expand_dims(img, 0)
		self.interpreter.set_tensor(self.input_details[0]['index'], img)				
		self.interpreter.invoke()			
		output = self.interpreter.get_tensor(self.output_details[0]['index'])
		output = np.squeeze(output)
		
		return output



def my_thread_1():
	print("Start threaded task 1")
	simulate_cpu_load()

	print("Task 1 completed")


def worker():
	while True:
		pass

def simulate_cpu_load():
	num_cores = multiprocessing.cpu_count()
	processes = []

	for _ in range(num_cores):
		p = multiprocessing.Process(target=worker)
		p.start()
		processes.append(p)

	time.sleep(3) 

	for p in processes:
		p.terminate()




if __name__ == '__main__':
	classifier_1 = ClassificationModel('mymodel.tflite)	
	
	cap = cv2.VideoCapture()
	for i in range(5):
		cap.open(i)
		if cap.isOpened():
			break

	if not cap.isOpened():
		print("Could not open camera")
		exit()


	try:
		while True:		
			# get image			
			ret, img = cap.read()

			# predict			
			p1 = classifier_1.predict(img)
			print(p1)			

			# threaded task
			if random() < 0.1:
				t = Thread(target=my_thread_1)
				t.start()
			
	except(KeyboardInterrupt):
		exit()  

 

0 项奖励
回复

2,347 次查看
FSet89
Contributor I

Hi, here is the code. I cannot share the model but you can try with any quantized tflite model.

 

import multiprocessing
from multiprocessing import Queue, Process
import numpy as np
from threading import Thread
from random import random, randint
import tflite_runtime.interpreter as tflite
import time
import cv2 
import os
import sys
import psutil

class ClassificationModel(object):
	def __init__(self, path, mask_path=None):
		self.interpreter = tflite.Interpreter(model_path=path)
		self.interpreter.allocate_tensors()
		self.input_details = self.interpreter.get_input_details()
		self.output_details = self.interpreter.get_output_details()
		self.input_shape = self.input_details[0]['shape']



	def predict(self, img, resize=True):

		if resize:
			img = cv2.resize(img, (self.input_shape[2], self.input_shape[1]))		

		img = (img/255.0).astype(np.float32)
		img = np.expand_dims(img, 0)
		self.interpreter.set_tensor(self.input_details[0]['index'], img)				
		self.interpreter.invoke()			
		output = self.interpreter.get_tensor(self.output_details[0]['index'])
		output = np.squeeze(output)
		
		return output



def my_thread_1():
	print("Start threaded task 1")
	simulate_cpu_load()

	print("Task 1 completed")


def worker():
	while True:
		pass

def simulate_cpu_load():
	num_cores = multiprocessing.cpu_count()
	processes = []

	for _ in range(num_cores):
		p = multiprocessing.Process(target=worker)
		p.start()
		processes.append(p)

	time.sleep(3) 

	for p in processes:
		p.terminate()




if __name__ == '__main__':
	classifier_1 = ClassificationModel('mymodel.tflite)	
	
	cap = cv2.VideoCapture()
	for i in range(5):
		cap.open(i)
		if cap.isOpened():
			break

	if not cap.isOpened():
		print("Could not open camera")
		exit()


	try:
		while True:		
			# get image			
			ret, img = cap.read()

			# predict			
			p1 = classifier_1.predict(img)
			print(p1)			

			# threaded task
			if random() < 0.1:
				t = Thread(target=my_thread_1)
				t.start()
			
	except(KeyboardInterrupt):
		exit()
0 项奖励
回复