tflite + XNNPACK delegate for inference on quantized network not working

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

tflite + XNNPACK delegate for inference on quantized network not working

2,572 次查看
edouard_charvet
Contributor III

Hello,

Running on i.mx8QM MEK board, with Yocto Linux LF5.15.71_2.2.0

Following the I.MX Machine Learning User Guide §3.7 to benchmark inference of TFLite using XNNPACK delegate with the example model mobilenet_v1_1.0_224_quant.tflite, I see that XNNPACK delegate is not being used for the inference (most likely because this is a quantized network - as it works fine with fp32 models).

Browsing the web a little bit, it sounds like XNNPACK supports quantized networks since Sept 2021 (cf https://blog.tensorflow.org/2021/09/faster-quantized-inference-with-xnnpack.html).

Is it possible and if so how can I get the XNNPACK delegate to work with quantized networks ? I guess I need to change something somewhere in the yocto linux build scripts... but what and where ?

Thanks

0 项奖励
回复
1 回复

2,561 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

You have to check the deepview https://www.nxp.com/design/software/development-software/eiq-ml-development-environment/eiq-inferenc...

Since not all images quantized works it have to be int8 delegate but the fp32 do not.

Regards

0 项奖励
回复