I flashed the Ubuntu image from https://www.ipi.wiki/pages/downloads-imx8mplus into the SD card and boot loader settings of the IMX8MP dev board [ I-Pi SMARC plus 51-77A07-0A30] to the SD card (0110). I am facing a few issues stated below:
1) I observe the processor slows down while doing normal operations like opening a folder, a terminal, or even displaying the desktop after login.
2) I was trying to install ros2 focal https://docs.ros.org/en/humble/Installation/Alternatives/Ubuntu-Development-Setup.html, but I run into an issue with low space on the device and could not complete the installation.
3) Since the ros2 installation needs internet data, when I try to connect an ethernet or a USB-based internet connection, the system becomes very slow and hangs sometimes, in this case, I have to reset the kit.
4) I am unable to connect to the wifi, the device recognizes the wifi modules around but fails to connect.
I would like to get some support here, can someone please guide me? thank you in advance.
Hello,
In this case you have to wirte to https://www.ipi.wiki/pages/downloads-imx8mplus since the image is from them.
Regards
Okay, thank you for your response.