test vectors for SCC (security controller) in non-secure mode

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

test vectors for SCC (security controller) in non-secure mode

1,936 次查看
martinkaiser
Contributor I

Dear all,

I'm looking at the SCC in an i.MX258 chipset. For now, I'm using non-secure mode (preferably in 3DES).

Do you have any test vectors (input data, iv for 3des and corresponding output data) that I could use to verify my calculations?

Best regards,

Martin

标签 (1)
0 项奖励
回复
3 回复数

1,813 次查看
martinkaiser
Contributor I

Hi Igor and Yuri,

thanks for your responses.

Actually, I was looking for samples of input data and corresponding output data for the published test key. My hope was that I could then do the exact same calculation with OpenSSL and get a better idea how the 3des engine works internally.

I managed to get this to work meanwhile so the issue is solved for me.

Regards,

Martin

0 项奖励
回复

1,813 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Martin

in general i.MX25 SCC tests are described in pdk2009_12_imx25_Linux_RM.pdf

Chapter 19 Security Drivers IMX25_0912_SDK_LINUXDOCS_BUNDLE

code examples in ltib (L2.6.31_09.12.00_SDK_SOURCE) imx-test package :

imx-test-09.12.00/module_test/scc_test_driver.c

Best regards

igor

0 项奖励
回复

1,813 次查看
Yuri
NXP Employee
NXP Employee

  Triple-DES tests are described in NIST Special Publication :
“Modes of Operation Validation System for the Triple Data Encryption
Algorithm (TMOVS): Requirements and Procedures”.
An additional test, the Multi-block Message Text (MMT), is also required.


http://csrc.nist.gov/publications/nistpubs/800-20/800-20.pdf

http://csrc.nist.gov/groups/STM/cavp/

  Also, let me remind, for i.MX25 "in non-secure mode [...] the decryption engine is available
for test purposes only with a default 168-bit 3DES ...".


Have a great day,
Yuri.

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复