target toolchain

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

target toolchain

1,789 Views
sachindhoundiya
Contributor II

Hello Yuri ,

Right now i compiled code in eclipse and copy output file in memory card. then run the output file in i.mx6ull.

Is there any toolchain to compile in imx6ull for c code. so that we have not to do copy in memory card the output file.

0 Kudos
Reply
1 Reply

1,381 Views
Yuri
NXP Employee
NXP Employee

Hello,

  You should provide the toolchain to Your target.

 

install gcc and toolchain on target rfs 

 

Creating a custom distribution image with Yocto for the RIoTboard  

 

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply