tamper pin IMX6Q

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

tamper pin IMX6Q

1,483 Views
marcomaioli
Contributor II

Hello,

we're using an iMX6Dual based board with linux 5.4.129 and we'd like to enable
tamper detection on pad TAMPER (signal SNVS_TAMPER).

Looking into the driver linux/drivers/crypto/caam/secvio.c it seems to us that
LP registers are never touched... so we're puzzled to know how the
"external-pin-tamper" in the driver should take effect!

Is this the right driver to use or we needed something different? We move the
signal on pad TAMPER but no IRQs arrive....

Thanks in advance,

0 Kudos
Reply
1 Reply

1,465 Views
art
NXP Employee
NXP Employee

The external tamper functionality is not implemented in the Linux BSP for i.MX6Dual/Quad processor.

Best Regards,
Artur

0 Kudos
Reply