systemd with ttymxc0

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

systemd with ttymxc0

跳至解决方案
5,729 次查看
kunyichen
Contributor IV

hi,

    I try the below on v3.14.52_v1.1.0qa bsp,

because I need to use connman with WIFI

so add 'systemd' into DISTRO_FEATURES

currently connman work well with WIFI

but I can't use serial console (ttymxc0) to login my system now after add systemd

I have try this systemd for Administrators, Part XVI , but still failed

have anyone can tell me, how to login by ttymxc0?

标签 (1)
标记 (3)
0 项奖励
回复
1 解答
4,027 次查看
kunyichen
Contributor IV

okay, currently workable when to enable CONFIG_FHANDLE of kernel

在原帖中查看解决方案

0 项奖励
回复
2 回复数
4,027 次查看
kunyichen
Contributor IV

when I booting into system then open a terminal to run below command will work,

systemctl enable [email protected]

but system booting still failed, check boot status

systemctl status [email protected]

will show Active: inactive(dead)

Dependency failed for Serial Getty on ttymxc0

Job [email protected] start failed with result 'dependency'

0 项奖励
回复
4,028 次查看
kunyichen
Contributor IV

okay, currently workable when to enable CONFIG_FHANDLE of kernel

0 项奖励
回复