support for docker on i.MX8MP

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

support for docker on i.MX8MP

1,542 次查看
SachinMR
Contributor I

Hi,
We are trying to bring up docker on imx8m plus device, by including meta virtualization layer in the yocto image build, by following below steps:
1. Clone the meta-virtualization layer in sources directory
git clone https://git.yoctoproject.org/git/meta-virtualization

2. making changes in the “conf/bblayers.conf” by adding the following line
BBLAYERS += "${BSPDIR}/sources/meta-virtualization"

3. Add the following lines in “conf/local.conf” file
DISTRO_FEATURES_append = " virtualization"
IMAGE_INSTALL_append = " docker-ce".

4. Building the image using bitbake command.

But the docker command is not being recognized even after booting the board with the new image.

Could you please let us know whether including docker in yocto image is supported on imx8m plus device.

0 项奖励
回复
1 回复

1,537 次查看
Zhiming_Liu
NXP TechSupport
NXP TechSupport

You can see this test docker image and it's readme:

https://hub.docker.com/repository/docker/fdsgfn/ubuntu21.04_imx

0 项奖励
回复