i.MX8MQ is having kernel panic

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX8MQ is having kernel panic

2,807 Views
harshitshah
Contributor III

Hi Team,

We are using the i.MX8MQ based board, during boot-up we have found that it is giving below kernel crash.

We are using i.MX8MQ processor custom board on L5.4.3_1.0.0 version. (We are not planning to modify the same if this is not a known issue).

 

===============================================================================

[2021-12-16 10:25:01] [   69.370450] Unable to handle kernel paging request at virtual address ffff8000eabac000
[2021-12-16 10:25:01] [   69.378373] Mem abort info:
[2021-12-16 10:25:01] [   69.381164]   ESR = 0x86000005
[2021-12-16 10:25:01] [   69.384216]   EC = 0x21: IABT (current EL), IL = 32 bits
[2021-12-16 10:25:01] [   69.389525]   SET = 0, FnV = 0
[2021-12-16 10:25:01] [   69.392576]   EA = 0, S1PTW = 0
[2021-12-16 10:25:01] [   69.395716] swapper pgtable: 4k pages, 48-bit VAs, pgdp=0000000041992000
[2021-12-16 10:25:01] [   69.402414] [ffff8000eabac000] pgd=000000013ffff003, pud=0000000000000000
[2021-12-16 10:25:01] [   69.409203] Internal error: Oops: 86000005 [#1] PREEMPT SMP
[2021-12-16 10:25:01] [   69.414773] Modules linked in:
[2021-12-16 10:25:01] [   69.417830] CPU: 1 PID: 0 Comm: swapper/1 Not tainted 5.4.3-lts-lf-5.4.y+gf811858 #1
[2021-12-16 10:25:01] [   69.425569] Hardware name: i.MX8MQ Processor (DT)
[2021-12-16 10:25:01] [   69.431660] pstate: 80000085 (Nzcv daIf -PAN -UAO)
[2021-12-16 10:25:01] [   69.436453] pc : 0xffff8000eabac000
[2021-12-16 10:25:01] [   69.439946] lr : ktime_get+0x40/0x98
[2021-12-16 10:25:01] [   69.443517] sp : ffff80001511bef0
[2021-12-16 10:25:01] [   69.446829] x29: ffff80001511bef0 x28: 0000000000000000 
[2021-12-16 10:25:01] [   69.452138] x27: 0000000000000000 x26: 0000000000000000 
[2021-12-16 10:25:01] [   69.457448] x25: 0000000000000000 x24: 0000000000000000 
[2021-12-16 10:25:01] [   69.462758] x23: ffff0000f80c1c00 x22: 00000000000060ba 
[2021-12-16 10:25:01] [   69.468068] x21: 0000000fed0e376b x20: ffff800014f11b00 
[2021-12-16 10:25:01] [   69.473377] x19: ffff0000ff791d70 x18: ffff0000f3234600 
[2021-12-16 10:25:01] [   69.478687] x17: 0000000000000000 x16: 0000000000000000 
[2021-12-16 10:25:01] [   69.483997] x15: ffff0000f20b3f80 x14: 0000000040000010 
[2021-12-16 10:25:01] [   69.489307] x13: ffff0000ff750000 x12: 0000000000000001 
[2021-12-16 10:25:01] [   69.494616] x11: 0000000000000000 x10: 00000000000009c0 
[2021-12-16 10:25:01] [   69.499926] x9 : ffff80001511be90 x8 : ffff0000f80c2620 
[2021-12-16 10:25:01] [   69.505236] x7 : 0000000000000000 x6 : ffff0000f83a46f0 
[2021-12-16 10:25:01] [   69.510546] x5 : 0000000000000007 x4 : 0000000000000000 
[2021-12-16 10:25:01] [   69.515855] x3 : ffff800010c7d140 x2 : 0000000000000000 
[2021-12-16 10:25:01] [   69.521165] x1 : ffff8000eabac000 x0 : ffff800014e9ff28 
[2021-12-16 10:25:01] [   69.526476] Call trace:
[2021-12-16 10:25:01] [   69.528920]  0xffff8000eabac000
[2021-12-16 10:25:01] [   69.532063]  tick_nohz_idle_enter+0x3c/0x70
[2021-12-16 10:25:01] [   69.536246]  do_idle+0x34/0x280
[2021-12-16 10:25:01] [   69.539386]  cpu_startup_entry+0x24/0x40
[2021-12-16 10:25:01] [   69.543310]  secondary_start_kernel+0x154/0x190
[2021-12-16 10:25:01] [   69.547844] Code: bad PC value
[2021-12-16 10:25:01] [   69.550903] ---[ end trace bc3e5a44512dce5e ]---
[2021-12-16 10:25:01] [   69.555520] Kernel panic - not syncing: Attempted to kill the idle task!
[2021-12-16 10:25:01] [   69.562219] SMP: stopping secondary CPUs
[2021-12-16 10:25:01] [   69.566146] Kernel Offset: disabled
[2021-12-16 10:25:01] [   69.569633] CPU features: 0x0002,2000200c
[2021-12-16 10:25:01] [   69.573639] Memory Limit: none
[2021-12-16 10:25:01] [   69.576695] Rebooting in 10 seconds..
[2021-12-16 10:25:13]

===============================================================================

[2021-12-16 10:26:39] [   79.198401] Unable to handle kernel paging request at virtual address ffff80001582c570
[2021-12-16 10:26:39] [   79.206324] Mem abort info:
[2021-12-16 10:26:39] [   79.209115]   ESR = 0x96000007
[2021-12-16 10:26:39] [   79.212168]   EC = 0x25: DABT (current EL), IL = 32 bits
[2021-12-16 10:26:39] [   79.217476]   SET = 0, FnV = 0
[2021-12-16 10:26:39] [   79.220528]   EA = 0, S1PTW = 0
[2021-12-16 10:26:39] [   79.223665] Data abort info:
[2021-12-16 10:26:39] [   79.226542]   ISV = 0, ISS = 0x00000007
[2021-12-16 10:26:39] [   79.230374]   CM = 0, WnR = 0
[2021-12-16 10:26:39] [   79.233341] swapper pgtable: 4k pages, 48-bit VAs, pgdp=0000000041992000
[2021-12-16 10:26:39] [   79.240038] [ffff80001582c570] pgd=000000013ffff003, pud=000000013fffe003, pmd=0000000132307003, pte=0000000000000000
[2021-12-16 10:26:39] [   79.250649] Internal error: Oops: 96000007 [#1] PREEMPT SMP
[2021-12-16 10:26:39] [   79.256219] Modules linked in:
[2021-12-16 10:26:39] [   79.259276] CPU: 0 PID: 309 Comm: 30902000.jr-eng Not tainted 5.4.3-lts-lf-5.4.y+gf811858 #1
[2021-12-16 10:26:39] [   79.267709] Hardware name: i.MX8MQ Processor (DT)
[2021-12-16 10:26:39] [   79.273800] pstate: 80000085 (Nzcv daIf -PAN -UAO)
[2021-12-16 10:26:39] [   79.278597] pc : pick_next_task_idle+0x30/0x48
[2021-12-16 10:26:39] [   79.283039] lr : pick_next_task_idle+0x2c/0x48
[2021-12-16 10:26:39] [   79.287479] sp : ffff80001582bd60
[2021-12-16 10:26:39] [   79.290791] x29: ffff80001582bd60 x28: 0000000000000000 
[2021-12-16 10:26:39] [   79.296101] x27: ffff80001582bde0 x26: ffff0000f8372180 
[2021-12-16 10:26:39] [   79.301410] x25: ffff800010fa5ff0 x24: ffff800010f6fc98 
[2021-12-16 10:26:39] [   79.306720] x23: ffff0000f8371c00 x22: ffff800014bdd018 
[2021-12-16 10:26:39] [   79.312030] x21: 0000000000000000 x20: ffff0000f8371c00 
[2021-12-16 10:26:39] [   79.317340] x19: ffff800014dd1e40 x18: 0000000000000358 
[2021-12-16 10:26:39] [   79.322649] x17: 0000000000000000 x16: 0000000000000000 
[2021-12-16 10:26:39] [   79.327959] x15: 0000000000000000 x14: 0000000040000010 
[2021-12-16 10:26:39] [   79.333268] x13: 0000000000000000 x12: 0000000000004722 
[2021-12-16 10:26:39] [   79.338578] x11: 00000000000001d7 x10: 00000000011ce9bc 
[2021-12-16 10:26:39] [   79.343888] x9 : 0000000000004722 x8 : 0000000000000000 
[2021-12-16 10:26:39] [   79.349197] x7 : 0000000000000000 x6 : ffff0000f8371cf0 
[2021-12-16 10:26:39] [   79.354507] x5 : 00000000ffffffff x4 : 0000000000000000 
[2021-12-16 10:26:39] [   79.359816] x3 : ffff800010114bd8 x2 : ffff800010119540 
[2021-12-16 10:26:39] [   79.365126] x1 : 0000000000000000 x0 : ffff800014dd1e40 
[2021-12-16 10:26:39] [   79.370436] Call trace:
[2021-12-16 10:26:39] [   79.372882]  pick_next_task_idle+0x30/0x48
[2021-12-16 10:26:39] [   79.376978]  __schedule+0x3d4/0x560
[2021-12-16 10:26:39] [   79.380464]  schedule+0x40/0xe0
[2021-12-16 10:26:39] [   79.383607]  kthread_worker_fn+0xf8/0x188
[2021-12-16 10:26:39] [   79.387614]  kthread+0xf0/0x120
[2021-12-16 10:26:39] [   79.390756]  ret_from_fork+0x10/0x18
[2021-12-16 10:26:39] [   79.394334] Code: f9404022 f9401c42 d63f0040 aa1303e0 (f9400bf3) 
[2021-12-16 10:26:39] [   79.400426] ---[ end trace 5d29fc571c53c860 ]---
[2021-12-16 10:26:39] [   79.405042] note: 30902000.jr-eng[309] exited with preempt_count 2

 

 

What can be the reason for the same? We have followed the hardware guidelines mentioned in the document and performed the DDR calibration. 

 

Regards.

Labels (1)
0 Kudos
Reply
3 Replies

2,794 Views
jimmychan
NXP TechSupport
NXP TechSupport

How many boards have this issue? Is the crash randomly? or crash at the same place during boot? Is the DDR stress test passed?

0 Kudos
Reply

2,788 Views
harshitshah
Contributor III

Hi @jimmychan ,

 

There are 3 boards that have this issue out of 15. This crash is happening at the same boot-up, and we are not getting the fs prompt.

Yes, DDR stress test in the overnight case is passing. 

Regards.

0 Kudos
Reply

2,785 Views
jimmychan
NXP TechSupport
NXP TechSupport

Could you provide the full boot up log of the good board and the failed board?

0 Kudos
Reply