streaming audio using gst-launch

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

streaming audio using gst-launch

17,246 Views
hr1z
Contributor I

I currently have a i.MX53 evaluation board. I can build gstreamer pipelines (using gst-launch) to send audio over the network to a remote machine. This works fine, but no matter what kind of combination I use (whether using freescale libraries or not) I cannot hear incoming network streams. I can play files locally no problem so it is not anything to do with the audio path.

Can someone post a sample of a working inbound network stream?

 

Thanks in advance.

Tags (1)
0 Kudos
Reply
17 Replies

12,534 Views
Kirill
Contributor I

thanks for replies!

0 Kudos
Reply

12,534 Views
RandyKrakora
NXP Employee
NXP Employee

Look for this "MX53_QSB_UBUNTU_SD_DEMO_IMAGE" here:http://www.freescale.com/imxquickstart


cai cx said:

Hi Randy

 I just can find L2.6.35_MX53_ER_1109_IMAGE or UBUNTU_RFS_DEMOIMG_1101 for QSB, but can't find "11.09 Ubuntu image" that you mentions, could you give me a website link?

 thanks.

0 Kudos
Reply

12,534 Views
RandyKrakora
NXP Employee
NXP Employee

Oh, then you probably need to use the package manager to install gstreamer, at least that's what it sounds like to me.

0 Kudos
Reply

12,534 Views
Kirill
Contributor I

No, I am compiling for my host Ubuntu (x86)

0 Kudos
Reply

12,534 Views
RandyKrakora
NXP Employee
NXP Employee

Are you building with ltib?

0 Kudos
Reply

12,534 Views
Kirill
Contributor I

thanks for reply! I already find that package, but on my Ubuntu 10.04 I faced some problems

"configure: Package gstreamer-0.10 was not found in the pkg-config search path.

Perhaps you should add the directory containing `gstreamer-0.10.pc'
to the PKG_CONFIG_PATH environment variable
No package 'gstreamer-0.10' found
configure: error: no gstreamer-0.10 >= 0.10.10.1 (GStreamer) found"

And dont know how to resolve it

0 Kudos
Reply

12,534 Views
RandyKrakora
NXP Employee
NXP Employee

Looks like they are both in gstreamer-plugins-good:

http://gstreamer.freedesktop.org/documentation/plugins.html

0 Kudos
Reply

12,533 Views
Kirill
Contributor I

Hello!

WARNING: erroneous pipeline: no element "rtppcmudepay", which package owns it? 

The same with WARNING: erroneous pipeline: no element "rtpL16pay"

0 Kudos
Reply

12,534 Views
caicx
Contributor I

Hi Randy

 I just can find L2.6.35_MX53_ER_1109_IMAGE or UBUNTU_RFS_DEMOIMG_1101 for QSB, but can't find "11.09 Ubuntu image" that you mentions, could you give me a website link?

 thanks.

0 Kudos
Reply

12,534 Views
RandyKrakora
NXP Employee
NXP Employee

I got it resolved, I got a 11.09 Ubuntu image that had it already fixed and used it.

Using ltib, there's some gstreamer patches that need removed, remove all patches but these two in gst-plugins-base.spec :

Patch1 : %{name}-0.10.12-relink.patch
Patch2 : %{name}-rawvideo.patch

Or use this procedure to update a standard Ubuntu image with the fix, I did this, but it didn't fix it for me, there's probably a step is missing - I'll get back to it at some point I hope:

  1. apt-get remove gstreamer0.10-plugins-base
  2. apt-get update
  3. apt-get install gstreamer0.10-plugins-base gstreamer0.10-plugins-good gstreamer0.10-alsa

Oh, and here's my test server/client - you can change the ip address to stream across a network:

Server:

gst-launch -v audiotestsrc  ! audioconvert ! rtpL16pay ! udpsink host=127.0.0.1 port=1234 auto-multicast=true port=1234

 

Client:

gst-launch -v udpsrc multicast-group=127.0.0.1 port=1234 caps="application/x-rtp, media=(string)audio, channels=(int)1, clock-rate=(int)44100, encoding-name=(string)L16" ! gstrtpbin ! rtpL16depay ! audioconvert ! queue ! autoaudiosink

0 Kudos
Reply

12,534 Views
Rodrigue
NXP Employee
NXP Employee

Hi,

Same for me. works fine between 2 VMs, with QSB as a Tx (VM as Rx) and vice versa.

I am using the latest 1109 + patches from January on START-R

0 Kudos
Reply

12,534 Views
RandyKrakora
NXP Employee
NXP Employee

Did this ever get resolved? Can you post a solution? We're having a similar issue with streaming. Works fine on a VM, but not on the QSB...

0 Kudos
Reply

12,534 Views
hr1z
Contributor I

This is the pipeline example that I used:

On the MX53QSB: (Tx audio stream)

gst-launch alsasrc  ! mulawenc ! rtppcmupay ! queue ! udpsink host=$HOST_IP port=$HOST_PORT -v

 

On the HOST PC:(Rx audio stream)

gst-launch udpsrc port=$HOST_PORT caps="application/x-rtp, media=audio, clock-rate=8000, encoding-name=PCMU, payload=0, ssrc=1253488865, clock-base=3079727525, seqnum-base=32302" ! queue ! rtppcmudepay ! mulawdec ! audioconvert ! alsasink -v

 

The above example works fine (only from MX53 to PC).

I've tried same pipeline, changing and adding different pipeline parameters, but same result.

Any ideas?

Regads,

Haysam

0 Kudos
Reply

12,534 Views
fabio_estevam
NXP Employee
NXP Employee

What is the Gstreamer pipeline you use on the PC to receive the audio stream?

 

Can´t the same pipeline be used on the MX53QSB?

 

Regards,

 

Fabio Estevam

0 Kudos
Reply

12,534 Views
hr1z
Contributor I

Thanks for the reply Fabio.

Yes receiving audio stream from the PC works fine.

Receiving audio stream on the MX53 does not work. I've tried many pipeline scenarios. I believe there's is something broken (not hardware) on the audio input stream on the MX53. Do you have an example gst-launch pipeline that works?

 

Regards

Haysam

0 Kudos
Reply

12,534 Views
fabio_estevam
NXP Employee
NXP Employee

Can you please try to receive the stream on a PC?

 

I would suggest you to try receiving the audio stream from a PC first; After that you can use the same pipeline on the MX53.

 

If you find issues also on the PC, please post this question on the gstreamer-devel mailing list, so that someone can assist you.

 

Regards,

 

Fabio Estevam

0 Kudos
Reply

12,534 Views
hr1z
Contributor I

Anybody been able to receive audio streams from a udp source and play with alsa using gst-launch?

I've tried many ways but nothing...

I suspect the gstreamer provided by freescale is broken.

0 Kudos
Reply