ssp slave

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

ssp slave

3,311件の閲覧回数
tomi
Contributor I

hey

is there a more detailed hardware description for ssp ports in slave mode

for example wich chip select is needed ..

tom

ラベル(1)
0 件の賞賛
返信
5 返答(返信)

3,047件の閲覧回数
YixingKong
Senior Contributor IV

Thomas, has Arthur's reply answered your question? If yes, please click Correct Answer, otherwise please keep working with Arthur. Please do not leave the DI there un-attended, as we will close Di in 3 days, if nothing happens.

Thanks,

Yixing

0 件の賞賛
返信

3,047件の閲覧回数
arthur_lai
Senior Contributor II

Hi Tom,

The SSP can work in a number of modes. How would you like to use the SSP?

Please check Table 17-1 on the reference manual and you should be able to find the info needed.

Thanks,

Arthur

0 件の賞賛
返信

3,047件の閲覧回数
tomi
Contributor I

sorry,

i want to use the ssp Port as spi slave and i can not find some detailed descriptions about it in the Userers manual.

0 件の賞賛
返信

3,047件の閲覧回数
YixingKong
Senior Contributor IV

Thomas,do you still have unresolved issues? If not, we will close the DI in 3 days.

Thanks,

Yixing

0 件の賞賛
返信

3,047件の閲覧回数
arthur_lai
Senior Contributor II

Hi Thomas,

For SPI signals assignment, you can refer to Table 17-1 on the Reference Manual.

The hardware connections are basically the same for either master or slave mode. The difference is that i.MX28 SCK, MOSI and SSn0 are input pins in slave mode.

Thanks,

Arthur