ssi can't generate bit clock

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

ssi can't generate bit clock

2,363 次查看
剑明廖
Contributor I

I configure ssi1 as network mode,Frame Sync and Transmit Clock generated internally,and route it to AUD3,but I can't get clock on AUD3_TXC pin and  AUD3_TXFS pin,who can help me?!!!!

Thanks in advance!!!

Is there any problem in this function?

//route ssi1 to AUD3

static int imx_audmux_config(int slave, int master)

{   

    int ret;

    unsigned int ptcr, pdcr;

    slave = slave - 1;          //slave=3-1

    master = master - 1;        //master=1-1

    ptcr = MXC_AUDMUX_V2_PTCR_SYN |

    MXC_AUDMUX_V2_PTCR_TFSDIR |    

    MXC_AUDMUX_V2_PTCR_TFSEL(master) |

    MXC_AUDMUX_V2_PTCR_TCLKDIR |

    MXC_AUDMUX_V2_PTCR_TCSEL(master);

    pdcr = MXC_AUDMUX_V2_PDCR_RXDSEL(master);

    ret = mxc_audmux_v2_configure_port(slave, ptcr, pdcr);

    ptcr = MXC_AUDMUX_V2_PTCR_SYN;

    pdcr = MXC_AUDMUX_V2_PDCR_RXDSEL(slave);

    ret = mxc_audmux_v2_configure_port(master, ptcr, pdcr);

    return 0;

}

标签 (2)
0 项奖励
回复
5 回复数

1,952 次查看
art
NXP Employee
NXP Employee

Actually, the code you listed here has no sense for me. As far as I understand, you are trying to configure the SSI1 interface to operate in master mode and to be routed out of the chip through AUD3 port. Am I right? Please clarify. Also, please specify, what exactly processor of i.MX series do you use to make me able to check the required configuration.


Have a great day,
Artur

0 项奖励
回复

1,952 次查看
剑明廖
Contributor I

Thank you very much!

Yes,you are right.And I use I.MX6Q processor.Please help me!

0 项奖励
回复

1,952 次查看
剑明廖
Contributor I

can any one help me?

0 项奖励
回复

1,952 次查看
saurabh206
Senior Contributor III

Hi

Have you setup  "snd_soc_dai_set_sysclk" correctly?

For SSI master mode you need to mentioned "SND_SOC_CLOCK_OUT"

ret = snd_soc_dai_set_sysclk(cpu_dai, 0, bclk, SND_SOC_CLOCK_OUT);

Thanks

Saurabh

0 项奖励
回复

1,952 次查看
剑明廖
Contributor I

I am sure that I have configure the sysclk as SND_SOC_CLOCK_OUT,but it still not clock generare on aud3.

Please help me, thank you very much!

0 项奖励
回复