splashscreen on android os

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

splashscreen on android os

2,111 Views
sachusanal
Contributor III

Dear Sir,

I am using Android lolipop source for  IMX6qsabresdp board .

I build the images by using user guide .

I need to set my custom splash screen on android booting.

now my image shows boot loader loading time free scale semiconductor then shows kernel tux then shows android at the time of kernel and file system booting.

could you please help me to change these three images and load my  custom splash image please help me.

Regards

Sachu

Labels (1)
0 Kudos
Reply
4 Replies

1,915 Views
sachusanal
Contributor III

Hello sir ,

could you please help me to set splash image on lolipop board.

from where i can store my spalsh screen image

0 Kudos
Reply

1,915 Views
igorpadykov
NXP Employee
NXP Employee

also it may be useful to look at attached  L5.0

Android_User's_Guide.pdf p.23.

Best regards

igor

0 Kudos
Reply

1,915 Views
sachusanal
Contributor III

Dear Igor ,

Could u please help me to edit the boot image , which file i can edit for image changes.

its an urgent task , please help me

0 Kudos
Reply

1,915 Views
saurabh206
Senior Contributor III
0 Kudos
Reply