spinlock bad magic??

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

spinlock bad magic??

4,780件の閲覧回数
xiaolong_zhang
Contributor II

this is my app VKFrame log (print this log,my system hung;kernel3.0.35 ;Constant temperature 40℃):

BUG: spinlock bad magic on CPU#0, QThread/1441
lock: bf52aca8, .magic: 00000000, .owner: QThread/1441, .owner_cpu: 0
[<801046d0>] (unwind_backtrace+0x0/0xf8) from [<8032fb90>] (do_raw_spin_unlock+0x80/0xc4)
[<8032fb90>] (do_raw_spin_unlock+0x80/0xc4) from [<805e8e84>] (_raw_spin_unlock_irqrestore+0xc/0x38)
[<805e8e84>] (_raw_spin_unlock_irqrestore+0xc/0x38) from [<801c1010>] (poll_freewait+0x30/0xa0)
[<801c1010>] (poll_freewait+0x30/0xa0) from [<801c2278>] (do_sys_poll+0x350/0x410)
[<801c2278>] (do_sys_poll+0x350/0x410) from [<801c23e8>] (sys_poll+0x5c/0xcc)
[<801c23e8>] (sys_poll+0x5c/0xcc) from [<800fdf80>] (ret_fast_syscall+0x0/0x30)
*** glibc detected *** ./VKFrame: malloc(): memory corruption: 0x2d00e160 ***

what to be caused by  magic = 00000000? 

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

4,548件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi zhang

to avoid this message one can try to rebuild all image with custom

application from scratch. Also one can try with new kernels from nxp repository

linux-imx - i.MX Linux kernel 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

4,548件の閲覧回数
xiaolong_zhang
Contributor II

Hi igorpadykov
    There's a bunch of machines.Using the same kernel, there are two machines in the thermostat for testing. One will happen every 24 hours or so, and the other has no abnormality. How to eliminate hardware problems?

0 件の賞賛
返信

4,548件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi zhang

for every machine own image should be created, not recommended to use same binaries.

0 件の賞賛
返信