I would like to update that all the versions in https://github.com/nxp-imx/imx-manifest is not updated with the NXP hyper link, there are a lot of link which are based on source.codeaurora.org one such is the https://source.codeaurora.org/external/imx/aosp/platform/bootable/recovery/ which is present android automotive 11 based code.
I have seen many post in NXP with the same issue, for people who are trying to build for first time might not have a backup and need to manually make the changes which will be difficult. Kindly we request to look in to this issue.