source.codeaurora.org error is not resolved in case of all android versions

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

source.codeaurora.org error is not resolved in case of all android versions

330 Views
vinisha_k_r
Contributor I

I would like to update that all the versions in https://github.com/nxp-imx/imx-manifest is not updated with the NXP hyper link, there are a lot of link which are based on source.codeaurora.org one such is the https://source.codeaurora.org/external/imx/aosp/platform/bootable/recovery/ which is present android automotive 11 based code.

I have seen many post in NXP with the same issue, for people who are trying to build for first time might not have a backup and need to manually make the changes which will be difficult. Kindly we request to look in to this issue.

0 Kudos
1 Reply

305 Views
Harvey021
NXP TechSupport
NXP TechSupport

Hi @vinisha_k_r 

nxp-imx-android · GitHub and GitHub - nxp-imx/imx-manifest at imx-android-11 hope those links can help you.

 

Best regards

Harvey

0 Kudos