some term like "ipu1-di0","sin0" etc

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

some term like "ipu1-di0","sin0" etc

1,267 次查看
freescaleusr1
Contributor I

HI,

some terms like "ipu1-di0", "sin0",etc, in which file is there explanation for them,

these terms is used in dts file or bootargs like "ldb=sin0",  hope to find the  expanation of more terms similar to them,

so that know how to set parameter for lvds. looking forward to reply, thanks.

标签 (4)
0 项奖励
回复
1 回复

1,208 次查看
Yuri
NXP Employee
NXP Employee

Hello,

  The following may help.

linux-imx6/fsl_ipuv3_fb.txt at master · samnazarko/linux-imx6 · GitHub


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复