she_storage_create fails in lifecycle moved device (Lifecycle = 0x0080)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

she_storage_create fails in lifecycle moved device (Lifecycle = 0x0080)

806 次查看
vicky15
Contributor III

Hi ,

Currently I'm working for Program J32v, we are using IMX8 DX currently observing she_storage_create api is failing in lifecycle moved device (OEM closed) (Lifecycle = 0x0080), but it works fine in OEM open board  (Lifecycle = 0x0020).

Attaching the test program we tested in both scenarios.

Below are logs snippets.

Tested in OEM CLOSED board (Lifecycle = 0x0080)

 # ./she_test_v
nvm manager failed to start
Closed nvm session

Tested in OEM OPEN board (Lifecycle = 0x0020)

./tmp/she_test_v
she_storage_create ret:0x1
she_open_session handle:0xe442d0d0
she_cmd_load_key ret:0x0
she_cmd_enc_cbc ret:0x0
she_cmd_dec_cbc ret:0x0
she_close_session
Closed nvm session

Thanks

Vignesh Pandian

0 项奖励
回复
0 回复数