set read bl len failed !

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

set read bl len failed !

ソリューションへジャンプ
2,380件の閲覧回数
Xavier
Contributor III

I am developing a card based on i.MX535 processor. All seem good, but I encountered a problem with µSD on slot SD1. When U-boot tries to load Linux kernel image from the µSD to DDR, we have the message "set read bl len failed".

I tried to rescan the µSD (mmc rescan 0), but it fails.

Any idea ?


ラベル(2)
0 件の賞賛
返信
1 解決策
2,149件の閲覧回数
imxcommunitysco
Senior Contributor II

Are you able to see some clock signal comming out from SD interface after the mmc rescan command?. You could use a scope for this.

Try to use another device number on the SD.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,150件の閲覧回数
imxcommunitysco
Senior Contributor II

Are you able to see some clock signal comming out from SD interface after the mmc rescan command?. You could use a scope for this.

Try to use another device number on the SD.

0 件の賞賛
返信