secure boot on imx8m plus on Android14 BSP

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

secure boot on imx8m plus on Android14 BSP

3,030 Views
Suryashmichakraborty
Contributor I

I want to enable the secure boot on imx8m plus board with Android 14 BSP, such that the board will always boot on our signed keys only.

0 Kudos
Reply
7 Replies

2,109 Views
Suryashmichakraborty
Contributor I

I am unable to sign the correct image on my imx8m plus board after fusing the keys permanently on the board! 

0 Kudos
Reply

2,972 Views
joanxie
NXP TechSupport
NXP TechSupport
0 Kudos
Reply

2,921 Views
Suryashmichakraborty
Contributor I

I have followed the steps given in the PDF and generated the keys like: 

SRK1_sha256_1024_65537_v3_ca_key.der
SRK1_sha256_1024_65537_v3_ca_key.pem
SRK1_sha256_1024_65537_v3_usr_key.der
SRK1_sha256_1024_65537_v3_usr_key.pem
SRK1_sha256_2048_65537_v3_ca_key.der
SRK1_sha256_2048_65537_v3_ca_key.pem
SRK2_sha256_1024_65537_v3_ca_key.der
SRK2_sha256_1024_65537_v3_ca_key.pem
SRK2_sha256_2048_65537_v3_ca_key.der
SRK2_sha256_2048_65537_v3_ca_key.pem
SRK3_sha256_2048_65537_v3_ca_key.der
SRK3_sha256_2048_65537_v3_ca_key.pem
SRK4_sha256_2048_65537_v3_ca_key.der
SRK4_sha256_2048_65537_v3_ca_key.pem and also the CSF, IMG and CA.

the private keys are openssl x509 -in crts/SRK1_sha256_2048_65537_v3_ca_crt.pem -text -noout | grep Subject
Subject: CN = SRK1_sha256_2048_65537_v3_ca
Subject Public Key Info:
X509v3 Subject Key Identifier: 

openssl x509 -in crts/CSF1_1_sha256_2048_65537_v3_usr_crt.pem -text -noout | grep Issuer
Issuer: CN = SRK1_sha256_2048_65537_v3_ca

openssl rsa -in keys/SRK1_sha256_2048_65537_v3_ca_key.pem -check
Enter pass phrase for keys/SRK1_sha256_2048_65537_v3_ca_key.pem:
RSA key ok

Are all these keys ready to flash on imx8m plus smarc som?

 

0 Kudos
Reply

2,728 Views
joanxie
NXP TechSupport
NXP TechSupport

did you generate SRK table already?

0 Kudos
Reply

2,662 Views
Suryashmichakraborty
Contributor I

yes,SRK Hash TableSRK Hash Table the SRK Hash table is generated successfully from the keys

0 Kudos
Reply

2,363 Views
joanxie
NXP TechSupport
NXP TechSupport

ok, then you can refer to the chapter 3.1.2.2 Signing bootloader images and 3.1.2.3 Signing the MCU firmware of enclosed file

0 Kudos
Reply

2,215 Views
Suryashmichakraborty
Contributor I

I have burned the fuses on my imx8m plus board, but unable to get the signed image or flashing, WhatsApp Image 2026-02-03 at 4.53.55 PM.jpeghex.jpgflash.jpg

how to recover and find the correct igned image for flashig?

0 Kudos
Reply