secure boot issure

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

secure boot issure

1,446件の閲覧回数
llliu
Contributor I

I have closed my device and secured my device ,hab_status shows that Secure boot enabled.I have downloaded a signed u-boot.imx ,but why I can download a no signed boot.img .It's not secure.I think a signed u-boot.imx can't load a no signed boot.img.Anyone can help me.Thank you!

0 件の賞賛
返信
1 返信

1,361件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

  In the secure close mode, it is possible to load an image, at least to check it.

But it is not possible to run unsigned image. Boot ROM does not allow to run

unsigned U-boot; further responsibility for verifying and running applications

under U-boot belongs to the U-boot. 


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信