secure boot issure

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

secure boot issure

1,471 Views
llliu
Contributor I

I have closed my device and secured my device ,hab_status shows that Secure boot enabled.I have downloaded a signed u-boot.imx ,but why I can download a no signed boot.img .It's not secure.I think a signed u-boot.imx can't load a no signed boot.img.Anyone can help me.Thank you!

0 Kudos
Reply
1 Reply

1,386 Views
Yuri
NXP Employee
NXP Employee

Hello,

  In the secure close mode, it is possible to load an image, at least to check it.

But it is not possible to run unsigned image. Boot ROM does not allow to run

unsigned U-boot; further responsibility for verifying and running applications

under U-boot belongs to the U-boot. 


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply