sdma firmware load

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

sdma firmware load

3,593件の閲覧回数
gaobo
Contributor I

Hi all:

kernel:4.14.78

machine:imx8mqevk

distro:fsl-imx-xwayland

rootfs:ubuntu 18.04

In the process of uboot loading the kernel,dmesg log follow:

pastedImage_1.png

Causing Bluetooth and Audio Card not to work properly,

pastedImage_2.png

pastedImage_3.png

please tell me that how to solve it,thanks!!!

0 件の賞賛
返信
5 返答(返信)

3,373件の閲覧回数
b36401
NXP Employee
NXP Employee

Please try to add IMAGE_INSTALL_append = " firmware-imx firmware-imx-sdma " into local.conf.

0 件の賞賛
返信

3,373件の閲覧回数
gaobo
Contributor I

First thanks for your reply.But I compile the kernel directly,then hang on ubuntu18.04 rootfs.I compile the kernel through bitbake in the yocto project.The operation steps are as follows:

MACHINE=imx8mqevk DISTRO=fsl-imx-xwayland source ./fsl-setup-release.sh -b bld-xwayland/

bitbake -c compile -f -v linux-imx 

bitbake linux-imx -c compile_kernelmodules -f -v

bitbake -c deploy -f -v linux-imx

then Replace the previous kernel with the generated kernel,mount Ubuntu18.04 rootfs。

please give me some advise,thanks!

0 件の賞賛
返信

3,373件の閲覧回数
b36401
NXP Employee
NXP Employee

Please make sure that you have right SDMA driver.

0 件の賞賛
返信

3,373件の閲覧回数
gaobo
Contributor I

pastedImage_1.png

pastedImage_2.png

in dts,success config

pastedImage_3.png

0 件の賞賛
返信

3,373件の閲覧回数
linux_downey
Contributor III

Hi gao bo:

   Have you solved this problem?

   I got the same error when I used the serial port .

@Victor Linnik

   Is there any solution? I  have checked the firmware as the same above.

Thanks. 

downey.

0 件の賞賛
返信