sdcard detect imx6

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

sdcard detect imx6

2,673 次查看
delauratfrançoi
Contributor II

Hello

My name is françois. I work with imx6dl sabre. I want to detect sdcard. I used udev to automount the sdcard and its work. But I want also that my personnal application detect the sdcard and I don't know how to do . Have you got a solution for me.

Thanks for All Help.

Best regards

François.

标签 (4)
标记 (1)
0 项奖励
回复
5 回复数

1,938 次查看
BiyongSUN
NXP Employee
NXP Employee

You need to study linux netlink knowledge.

0 项奖励
回复

1,938 次查看
delauratfrançoi
Contributor II

Hello

Thanks to reply.

I found the same solution:

#include <stdio.h>

#include <stdlib.h>

#include <string.h>

#include <unistd.h>

#include <pthread.h>

#include <mqueue.h>       // required for messages

#include <asm/types.h>

#include <sys/socket.h>

#include <linux/rtnetlink.h>

#include <linux/netlink.h>

void* SDcardManager_thread(void*)

{

    int ns = -1;

    struct sockaddr_nl sa;

    char buf[4096];

    struct iovec iov = { buf, sizeof(buf) };

    struct msghdr msg = { &sa, sizeof(sa), &iov, 1, NULL, 0, 0 };

    int len;

    memset (&sa, 0, sizeof(sa));

    sa.nl_family = AF_NETLINK;

    sa.nl_groups = RTMGRP_LINK | RTMGRP_IPV4_IFADDR;

    ns = socket(AF_NETLINK, SOCK_RAW, NETLINK_KOBJECT_UEVENT);

    if (ns < 0) {

            perror("socket()");

            ret=0;

    }//end if (ns < 0)

    if (bind(ns, (struct sockaddr*)&sa, sizeof(sa))) {

            perror("bind()");

            ret=0;

    }//end if (bind(ns, (struct sockaddr*)&sa, sizeof(sa)))

    while (ret) {

            len = recvmsg (ns, &msg, 0);

            if (len < 0) {

                    perror("recvmsg()");

                    break;

            }//fi(len < 0)

            buf[4095] = 0;

            if((strstr(buf,NAME_SD))!=NULL)

            {

                //sdcard add

                if((strstr(buf,NAME_ADD))!=NULL)

                {

                    //todo here your code

                }//if((strstr(buf,NAME_ADD))!=NULL)

                else

                {

                    //sdcard remove

                    if((strstr(buf,NAME_REMOVE))!=NULL)

                    {

                        //todo here your code

                    }//if((strstr(buf,NAME_REMOVE))!=NULL)

                }//else((strstr(buf,NAME_ADD))!=NULL)

            }//fi((strstr(buf,NAME_SD))!=NULL)

    }//end while

    return ((void*)&ret);

}

Best regards

François.

0 项奖励
回复

1,938 次查看
jimmychan
NXP TechSupport
NXP TechSupport

Sorry, I don't understand your question. As you can mount the sdcard, then sd card can be found in /dev/. (e.g. /dev/mmcblk0)  Would you tell me more detail about your problem? Have a nice day.

0 项奖励
回复

1,938 次查看
delauratfrançoi
Contributor II

Hello

Sorry to my question. Currently I used the udev system. I wrote a script to mount or umount sdcard. This script is called by udev. its work.

But now my application must know (to display an sdcard icone) if the sdcard is present or no. Indeed I can use the file /dev/mmcblk0. But I would like that my application is prevented by an interrupt or by a signal and I don't know that interrupt or signal use.

Have you got a solution for me

Thanks for All Help.

Best regards

François.

0 项奖励
回复

1,938 次查看
BiyongSUN
NXP Employee
NXP Employee

Netlink is how the udev is working. Which is the hook for the linux driver sending message to user space such as udev or mdev in busybox.

That is what I reply to you " You need to study linux netlink knowledge".

You can read udev source code, but big.

Also you can read the mdev source code in busybox, that is simple and small.

0 项奖励
回复