same RAM part number but different SOM Part numbers

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

same RAM part number but different SOM Part numbers

3,191件の閲覧回数
shamiullah
Contributor III

Hi everyone,

I am using MIMX8MM5DVTLZDA for NXP EVK IMX8MM and MIMX8MM3DVTLZAA for customized board.  we are using same part number RAM [MT53D512M32D2DS-053 WT:D] for both the above mentioned boards. we used the same DCD table in uboot for both the boards. But we are facing errors. Customized board is not completely booting . It is stopping middle of kernel . Please let us know for any modifications.

Please find the attached text file for logs

Thanks & Regards

Shamiullah

0 件の賞賛
返信
2 返答(返信)

3,186件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Shamiullah

 

for that issue may be recommended to run ddr test (use latest RPA tool) and rebuild image as

described in  MSCALE_DDR_Tool_User_Guide.pdf

https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX-8M-Family-DDR-Tool-Release/ta-p/110...

Also recommended to use latest nxp uboot/linux described on

https://www.nxp.com/design/software/embedded-software/i-mx-software/embedded-linux-for-i-mx-applicat...

 

Best regards
igor

0 件の賞賛
返信

3,166件の閲覧回数
shamiullah
Contributor III

Hi igor,

Thanks for the suggestion.

Followed MSCALE ddr tool user guide and generated custom uboot binary. 

ddr stress test gets success, but when i try to boot the custom board with newly generated uboot, it hangs at 

starting kernel ......

after this print i can see a garbage is printing on the console.

Please find the attachment for boot log

 

Thanks 

shami

0 件の賞賛
返信