rtl8192cufw_TMSC.bin missing

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

rtl8192cufw_TMSC.bin missing

4,897件の閲覧回数
skaicai
Contributor I

I purchased  USB WiFi adapters that is supposed to work on Linux (Realtek 8192 cu ). I am using IMX6Q android 5.1.1 with version 3.14.52 of the kernel. I have enabled the rlt8192cu driver in the kernel, compiled it and installed it on my board. When I boot the board and plug in the usb dongle the system sees it and tries to install it. However it then says it tries to install "alternalte" firmware. This is what I am seeing:

ci_hdrc ci_hdrc.0: EHCI Host Controller                                               

ci_hdrc ci_hdrc.0: new USB bus registered, assigned bus number 2                      

max8903-charger max8903.18: USB Charger Connected.                                    

ci_hdrc ci_hdrc.0: USB 2.0 started, EHCI 1.00

usb usb2: New USB device found, idVendor=1d6b, idProduct=0002

usb usb2: New USB device strings: Mfr=3, Product=2, SerialNumber=1

usb usb2: Product: EHCI Host Controller

usb usb2: Manufacturer: Linux 3.14.52 ehci_hcd

usb usb2: SerialNumber: ci_hdrc.0

hub 2-0:1.0: USB hub found

hub 2-0:1.0: 1 port detected

warning: `main' uses 32-bit capabilities (legacy support in use)

usb 2-1: new high-speed USB device number 2 using ci_hdrc

usb 2-1: New USB device found, idVendor=0bda, idProduct=8176

usb 2-1: New USB device strings: Mfr=1, Product=2, SerialNumber=3

usb 2-1: Product: 802.11n WLAN Adapter

usb 2-1: Manufacturer: Realtek

usb 2-1: SerialNumber: 00e04c000001

rtl8192cu: Chip version 0x10

rtl8192cu: MAC address: 00:13:ef:80:45:6b

rtl8192cu: Board Type 0

rtl_usb: rx_max_size 15360, rx_urb_num 8, in_ep 1

rtl8192cu: Loading firmware rtlwifi/rtl8192cufw_TMSC.bin

usb 2-1: Direct firmware load failed with error -2

usb 2-1: Falling back to user helper

usb 2-1: Direct firmware load failed with error -2

usb 2-1: Falling back to user helper

rtlwifi: Loading alternative firmware rtlwifi/rtl8192cufw.bin

rtlwifi: Firmware rtlwifi/rtl8192cufw_TMSC.bin not available

how can I fix this problem in imx6q android 5.1.1?

ラベル(2)
0 件の賞賛
返信
3 返答(返信)

3,436件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Skai

attempts to install "alternalte" firmware means

that this chip needs its specific firmware version, suggest

to apply to vendor of this chip for updated firmware.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

3,435件の閲覧回数
skaicai
Contributor I

The usb wifi is a small thing . I don't think the vendor will kindly provide the update confirm firmware for me. I download the rtl8192cufw_TMSC.bin from the internet , but it print this :rtl8192cu: Loading firmware rtlwifi/rtl8192cufw_TMSC.bin

direct firmware load failed with error -2.

So you can test the 8188 in your board for android 5.1 system ?

0 件の賞賛
返信

3,435件の閲覧回数
jaffinmk
Contributor III

Hi

Did you get a solution for "firmware loading failed"?? I downloaded the firmware from internet and copied it in the firmware folder but it doesnt load.

0 件の賞賛
返信