rtl8188eus

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

rtl8188eus

1,747 Views
hahhahha
Contributor I

   lsusb can see rtl8188eus device,but when i us ifconfig -a ,i can't see wlan0. why?Attached files is the log? i don't know why ?I use a usb rtl8188eus wlan card  ,use the USB_OTG2 which is used as a host port ,then through GL850 ,then to USB type a port ,5v of the port is always on .anybody can help me 

 

Labels (1)
0 Kudos
Reply
1 Reply

1,730 Views
igorpadykov
NXP Employee
NXP Employee
0 Kudos
Reply